ClearanceSet Class¶
-
class
NXOpen.Assemblies.
ClearanceSet
¶ Bases:
NXOpen.NXObject
Represents
NXOpen.Assemblies.ClearanceSet
.Input to this class can be PSM facet objects.
Currently we don’t support KF at this time.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CalculatePenetrationDepth | Calculate penetration depth for a set of hard interferences. |
Copy | Makes a copy of a dataset. |
CreateAttributeIterator | Create an attribute iterator |
CreateInterferenceGeometry | Construct interference geometry for a set of hard interferences. |
Delete | Delete this clearance set |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteInterference | Deletes the interference for a given object pair. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DetectObsoleteSettings | Detects whether a clearance set was defined with settings which are obsolete/no longer supported. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetInterferenceData | Inquires the data associated with a given pair of interfering objects. |
GetIsPairChanged | Inquires if an object pair has changed since the last analysis run. |
GetNextInterference | Cycles the interference in a clearance analysis data set. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNumberOfInterferences | Inquires the number of interferences stored in a clearance analysis data set. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetResults | Inquires a summary of the results of the most recent clearance analysis run. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetVersion | Gets the version of a clearance analysis dataset. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
PerformAnalysis | Perform an analysis on this clearance set with option to specify whether out-of-date excluded pairs will be reanalyzed. |
Prints a representation of this object to the system log file. | |
ReanalyzePairs | Reanalyze a set of interferences using the specified analysis method. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetInterferenceText | Associates a text string to an interfering object pair. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
ClearanceSetCopyMode Enumeration | Specify the dataset copy mode |
ClearanceSetInterferenceType Enumeration | Specify the type of interference |
ClearanceSetJobStatus Enumeration | Specify the job aborted status |
ClearanceSetPenetrationDepthResult Enumeration | The result of penetration depth calculation |
ClearanceSetReanalyzeOutOfDateExcludedPairs Enumeration | Specify whether to reanalyze out-of-date excluded pairs. |
ClearanceSetReanalyzePairCalculationMethod Enumeration | The analysis method to use when reanalyzing a pair. |
Structs¶
ClearanceSetSummary_Struct Struct | Summary of the most recent Clearance Analysis results |
Property Detail¶
IsOccurrence¶
-
ClearanceSet.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ClearanceSet.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ClearanceSet.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ClearanceSet.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ClearanceSet.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ClearanceSet.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CalculatePenetrationDepth¶
-
ClearanceSet.
CalculatePenetrationDepth
¶ Calculate penetration depth for a set of hard interferences.
The interferences must be specified using two parallel arrays: the objects in the first interference should be given in the first elements of the arrays, the objects in the second interference should be given in the second elements of the arrays, etc.
Signature
CalculatePenetrationDepth(firstObjects, secondObjects)
Parameters: - firstObjects (list of
NXOpen.DisplayableObject
) – The first object of each interference. Must be the same size as secondObjects. - secondObjects (list of
NXOpen.DisplayableObject
) – The second object of each interference. Must be the same size as firstObjects.
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- firstObjects (list of
Copy¶
-
ClearanceSet.
Copy
¶ Makes a copy of a dataset.
You must supply a unique name. There are three modes in which to copy the dataset:
NXOpen.Assemblies.ClearanceSetCopyMode.NoResults
only copies the setup data. The version of the new dataset is set to zero (meaning clearance analysis has not been run);NXOpen.Assemblies.ClearanceSetCopyMode.Results
makes a copy of the current analysis results, but not the interference bodies;NXOpen.Assemblies.ClearanceSetCopyMode.InterfBodies
makes a complete copy of the results. The name must be less than MAX_LINE_SIZE characters longSignature
Copy(name, mode)
Parameters: - name (str) – the name of the new dataset
- mode (
NXOpen.Assemblies.ClearanceSetCopyMode
) – copy mode
Returns: the dataset that is copied
Return type: New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
CreateInterferenceGeometry¶
-
ClearanceSet.
CreateInterferenceGeometry
¶ Construct interference geometry for a set of hard interferences.
The interferences must be specified using two parallel arrays: the objects in the first interference should be given in the first elements of the arrays, the objects in the second interference should be given in the second elements of the arrays, etc.
Signature
CreateInterferenceGeometry(firstObjects, secondObjects)
Parameters: - firstObjects (list of
NXOpen.DisplayableObject
) – The first object of each interference. Must be the same size as secondObjects. - secondObjects (list of
NXOpen.DisplayableObject
) – The second object of each interference. Must be the same size as firstObjects.
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- firstObjects (list of
Delete¶
-
ClearanceSet.
Delete
¶ Delete this clearance set
Signature
Delete()
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DeleteInterference¶
-
ClearanceSet.
DeleteInterference
¶ Deletes the interference for a given object pair.
Both objects must be members of the given data set. If the object pair does not refer to an existing interference, an error is returned. All data associated with the interference is deleted.
Signature
DeleteInterference(object1, object2)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object in the pair - object2 (
NXOpen.DisplayableObject
) – the second object in the pair
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
DetectObsoleteSettings¶
-
ClearanceSet.
DetectObsoleteSettings
¶ Detects whether a clearance set was defined with settings which are obsolete/no longer supported.
For example, prior to NX 9.0, an optional setting “ignore mated pairs” was available. Existing results may still be read from a clearance set with obsolete settings, but the next time analysis is performed, the obsolete settings will be removed and all existing results cleared. Optionally, this method can perform any required cleanup now, instead of waiting until the next analysis.
Signature
DetectObsoleteSettings(doCleanupNow)
Parameters: doCleanupNow (bool) – whether cleanup should be performed now Returns: whether the clearance set contains obsolete settings Return type: bool New in version NX10.0.2.
License requirements: assemblies (“ASSEMBLIES MODULE”)
FindObject¶
-
ClearanceSet.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetInterferenceData¶
-
ClearanceSet.
GetInterferenceData
¶ Inquires the data associated with a given pair of interfering objects.
Signature
GetInterferenceData(object1, object2)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object in the pair - object2 (
NXOpen.DisplayableObject
) – the second object in the pair
Returns: a tuple
Return type: A tuple consisting of (type, newInterference, interfBodies, point1, point2, text, interfNum, config, depthResult, depth, direction, minPoint, maxPoint). type is a
NXOpen.Assemblies.ClearanceSetInterferenceType
. the interference type newInterference is a bool. the flag for new interference interfBodies is a list ofNXOpen.DisplayableObject
. the list of interference bodies point1 is aNXOpen.Point3d
. a point on the first object point2 is aNXOpen.Point3d
. a point on the second object text is a str. text associated with the interference interfNum is a int. a unique number for the interference config is a int. the configuration index depthResult is a int. result status of penetration depth calculation depth is a float. depth of penetration direction is aNXOpen.Vector3d
. a unit vector indicating the direction of penetration minPoint is aNXOpen.Point3d
. the points on the interference region at the extremes of depth maxPoint is aNXOpen.Point3d
. the points on the interference region at the extremes of depthNew in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
GetIsPairChanged¶
-
ClearanceSet.
GetIsPairChanged
¶ Inquires if an object pair has changed since the last analysis run.
Both objects must be solid bodies or facet models that are members of the clearance analysis data set. If either object has changed since the last analysis run, then isChanged is returned as TRUE. If no analysis has been run on either of the objects, TRUE is returned.
Signature
GetIsPairChanged(object1, object2)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object in the pair - object2 (
NXOpen.DisplayableObject
) – the second object in the pair
Returns: Has this pair changed since the last analysis run?
Return type: bool
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
GetNextInterference¶
-
ClearanceSet.
GetNextInterference
¶ Cycles the interference in a clearance analysis data set.
Interferences are stored as object pairs. Start the cycling using None as the input values for both object1 and object2. This routine passes back the tags of the objects that define the next interference. None returned for either object indicates the end of the cycling.
Signature
GetNextInterference(object1, object2)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object in the pair of the current interference - object2 (
NXOpen.DisplayableObject
) – the second object in the pair of the current interference
Returns: a tuple
Return type: A tuple consisting of (nextObject1, nextObject2). nextObject1 is a
NXOpen.DisplayableObject
. the first object in the pair of the next interference nextObject2 is aNXOpen.DisplayableObject
. the second object in the pair of the next interferenceNew in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
GetNumberOfInterferences¶
-
ClearanceSet.
GetNumberOfInterferences
¶ Inquires the number of interferences stored in a clearance analysis data set.
If clearance analysis has never been run on the data set, an error is returned.
Signature
GetNumberOfInterferences()
Returns: the number of interferences associated with the dataset Return type: int New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetResults¶
-
ClearanceSet.
GetResults
¶ Inquires a summary of the results of the most recent clearance analysis run.
The
NXOpen.Assemblies.ClearanceSetSummary_Struct
structure is filled with analysis statistics, including numbers of objects, number of pairs, number of checked pairs, and number of interferences of each type. If clearance analysis has never been run on the data set, an error is returned.Signature
GetResults()
Returns: the summary structure Return type: NXOpen.Assemblies.ClearanceSetSummary_Struct
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetVersion¶
-
ClearanceSet.
GetVersion
¶ Gets the version of a clearance analysis dataset.
The version indicates how many times clearance analysis has been run on a data set. If the version is zero, then the analysis has never been run.
Signature
GetVersion()
Returns: Return type: int New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
PerformAnalysis¶
-
ClearanceSet.
PerformAnalysis
¶ Perform an analysis on this clearance set with option to specify whether out-of-date excluded pairs will be reanalyzed.
You can specify to use the Customer Default setting, or you can specify a true or false option to override the Customer Default.
Signature
PerformAnalysis(reanalyzeOption)
Parameters: reanalyzeOption ( NXOpen.Assemblies.ClearanceSetReanalyzeOutOfDateExcludedPairs
) –New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Print¶
-
ClearanceSet.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ReanalyzePairs¶
-
ClearanceSet.
ReanalyzePairs
¶ Reanalyze a set of interferences using the specified analysis method.
The interferences must be specified using two parallel arrays: the objects in the first interference should be given in the first elements of the arrays, the objects in the second interference should be given in the second elements of the arrays, etc.
Signature
ReanalyzePairs(firstObjects, secondObjects, calculationMethod)
Parameters: - firstObjects (list of
NXOpen.DisplayableObject
) – The first object of each interference. Must be the same size as secondObjects. - secondObjects (list of
NXOpen.DisplayableObject
) – The second object of each interference. Must be the same size as firstObjects. - calculationMethod (
NXOpen.Assemblies.ClearanceSetReanalyzePairCalculationMethod
) –
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- firstObjects (list of
SetInterferenceText¶
-
ClearanceSet.
SetInterferenceText
¶ Associates a text string to an interfering object pair.
Both objects must be members of the given dataset. If the object pair does not refer to an existing interference, an error is returned.
Signature
SetInterferenceText(object1, object2, text)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object in the pair - object2 (
NXOpen.DisplayableObject
) – the second object in the pair - text (str) – the name of the new dataset
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
SetName¶
-
ClearanceSet.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.