UserSymbolPreferences Class¶
-
class
NXOpen.Annotations.
UserSymbolPreferences
¶ Bases:
NXOpen.TransientObject
Represents preferences related to user-defined symbols
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetSize | Gets the size preference |
SetLengthAndHeight | Sets the length and height |
SetScaleAndAspectRatio | Sets the scale and aspect ratio |
Enumerations¶
UserSymbolPreferencesSizeType Enumeration | Specifies whether length and height or scale and aspect ratio is used in specifying the size of the symbol |
Method Detail¶
Dispose¶
-
UserSymbolPreferences.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetSize¶
-
UserSymbolPreferences.
GetSize
¶ Gets the size preference
Signature
GetSize()
Returns: a tuple Return type: A tuple consisting of (sizeType, lengthOrScale, heightOrAspectRatio). sizeType is a NXOpen.Annotations.UserSymbolPreferencesSizeType
. Specifies whether length and height or scale and aspect ratio is used lengthOrScale is a float. Length or scale heightOrAspectRatio is a float. Height or aspect ratioNew in version NX3.0.0.
License requirements: None.