UserSymbolPreferencesSizeType Enumeration¶
NXOpen.Annotations.UserSymbolPreferences.SizeType is an alias for NXOpen.Annotations.UserSymbolPreferencesSizeType
-
class
NXOpen.Annotations.
UserSymbolPreferencesSizeType
¶ Bases:
object
Specifies whether length and height or scale and aspect ratio is used in specifying the size of the symbol
Enum Members
Enum Member Enum Member Description LengthHeight length and height ScaleAspectRatio scale and aspect ratio -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-