SelectBaseCustomSymbolList Class¶
-
class
NXOpen.Annotations.
SelectBaseCustomSymbolList
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a list of objects on a selection list.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DuplicatesAllowed | Returns whether duplicate objects are allowed in the selection list. |
Size | Returns the number of objects in the list. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Add | Adds an object to the list |
Clear | Removes all items from the list. |
Contains | Returns whether the specified object is already in the list or not. |
GetArray | Returns the list of objects in the selection list. |
GetSelectObjectArray | Returns the list of SelectObjects in the selection list. |
Remove | Remove specified object from list. |
RemoveArray | Remove specified objects from list. |
SetArray | Sets the list of objects in the selection list. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DuplicatesAllowed¶
-
SelectBaseCustomSymbolList.
DuplicatesAllowed
¶ Returns whether duplicate objects are allowed in the selection list.
-------------------------------------
Getter Method
Signature
DuplicatesAllowed
Returns: Whether duplicate objects are allowed Return type: bool New in version NX5.0.0.
License requirements: None.
Method Detail¶
Add¶
-
SelectBaseCustomSymbolList.
Add
¶ Overloaded method Add
Add(object)
Add(objects)
Add(inputSelectionMethod)
Add(selection, view, point)
Add(snapType, selection1, view1, point1, selection2, view2, point2)
Add(selection, caeSubType, caeSubId)
-------------------------------------
Adds an object to the list
Signature
Add(object)
Parameters: object ( NXOpen.Annotations.BaseCustomSymbol
) – object to addReturns: True if succesully added to list; False if the object was already a member of the list and duplicates are not allowed :rtype: bool
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Adds a set of objects to the list
Signature
Add(objects)
Parameters: objects (list of NXOpen.Annotations.BaseCustomSymbol
) – objects to addReturns: True if succesully added all objects to the list; False if there was at least one object that was already a member of the list and duplicates are not allowed :rtype: bool
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Adds the objects from a SelectionMethod to the list
Signature
Add(inputSelectionMethod)
Parameters: inputSelectionMethod ( NXOpen.SelectionMethod
) – selection method containing objects to addReturns: True if succesully added all objects to the list; False if there was at least one object that was already a member of the list and duplicates are not allowed :rtype: bool
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Adds the object with the objects view and objects point
Signature
Add(selection, view, point)
Parameters: - selection (
NXOpen.Annotations.BaseCustomSymbol
) – selected object - view (
NXOpen.View
) – selected object view - point (
NXOpen.Point3d
) – selected object point
Returns: True if succesully added to list;
False if the object was already a member of the list and duplicates are not allowed :rtype: bool
New in version NX5.0.0.
License requirements: None.
-------------------------------------
The object being selected with the objects view and objects point and snap information.
Signature
Add(snapType, selection1, view1, point1, selection2, view2, point2)
Parameters: - snapType (
NXOpen.InferSnapTypeSnapType
) – snap point type - selection1 (
NXOpen.Annotations.BaseCustomSymbol
) – first selected object - view1 (
NXOpen.View
) – first selected object view - point1 (
NXOpen.Point3d
) – first selected object point - selection2 (
NXOpen.Annotations.BaseCustomSymbol
) – second selected object - view2 (
NXOpen.View
) – second selected object view - point2 (
NXOpen.Point3d
) – second selected object point
Returns: True if succesully added all objects to the list;
False if there was at least one object that was already a member of the list and duplicates are not allowed :rtype: bool
New in version NX5.0.0.
License requirements: None.
-------------------------------------
The object being selected with CAE set object information.
Signature
Add(selection, caeSubType, caeSubId)
Parameters: - selection (
NXOpen.Annotations.BaseCustomSymbol
) – selected object - caeSubType (
NXOpen.CaeObjectTypeCaeSubType
) – CAE set object sub type - caeSubId (int) – CAE set object sub id
Returns: True if succesully added all objects to the list;
False if there was at least one object that was already a member of the list and duplicates are not allowed :rtype: bool
New in version NX5.0.0.
Deprecated since version NX10.0.0: Use other versions of
NXOpen.SelectObjectList.Add()
.License requirements: None.
-------------------------------------
Clear¶
-
SelectBaseCustomSymbolList.
Clear
¶ Removes all items from the list.
Signature
Clear()
New in version NX5.0.0.
License requirements: None.
Contains¶
-
SelectBaseCustomSymbolList.
Contains
¶ Returns whether the specified object is already in the list or not.
Signature
Contains(object)
Parameters: object ( NXOpen.Annotations.BaseCustomSymbol
) – object to checkReturns: true if object is in the list, false otherwise Return type: bool New in version NX5.0.0.
License requirements: None.
GetArray¶
-
SelectBaseCustomSymbolList.
GetArray
¶ Overloaded method GetArray
GetArray()
GetArray()
-------------------------------------
Returns the list of objects in the selection list.
Signature
GetArray()
Returns: items in list Return type: list of NXOpen.Annotations.BaseCustomSymbol
New in version NX5.0.0.
License requirements: None.
-------------------------------------
GetSelectObjectArray¶
-
SelectBaseCustomSymbolList.
GetSelectObjectArray
¶ Returns the list of SelectObjects in the selection list.
Signature
GetSelectObjectArray()
Returns: items in list Return type: list of NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
Remove¶
-
SelectBaseCustomSymbolList.
Remove
¶ Overloaded method Remove
Remove(object)
Remove(object, view)
Remove(snapType, selection1, view1, point1, selection2, view2, point2)
Remove(inputSelectionMethod)
-------------------------------------
Remove specified object from list.
Signature
Remove(object)
Parameters: object ( NXOpen.Annotations.BaseCustomSymbol
) – Object to removeReturns: True if succesully removed from list; False if the object was not a member of the list :rtype: bool
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Remove specified object from list.
Signature
Remove(object, view)
Parameters: - object (
NXOpen.Annotations.BaseCustomSymbol
) – Object to remove - view (
NXOpen.View
) – with this view
Returns: True if succesully removed from list;
False if the object / view was not a member of the list :rtype: bool
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Remove specified object from list.
Signature
Remove(snapType, selection1, view1, point1, selection2, view2, point2)
Parameters: - snapType (
NXOpen.InferSnapTypeSnapType
) – snap point type - selection1 (
NXOpen.Annotations.BaseCustomSymbol
) – first selected object - view1 (
NXOpen.View
) – first selected object view - point1 (
NXOpen.Point3d
) – first selected object point - selection2 (
NXOpen.Annotations.BaseCustomSymbol
) – second selected object - view2 (
NXOpen.View
) – second selected object view - point2 (
NXOpen.Point3d
) – second selected object point
Returns: True if succesully removed from list;
False if the object was not a member of the list :rtype: bool
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Removes the objects from a SelectionMethod from the list
Signature
Remove(inputSelectionMethod)
Parameters: inputSelectionMethod ( NXOpen.SelectionMethod
) – selection method containing objects to addReturns: True if succesully removed all objects from the list; False if there was at least one object that was not a member of the list :rtype: bool
New in version NX6.0.0.
License requirements: None.
-------------------------------------
RemoveArray¶
-
SelectBaseCustomSymbolList.
RemoveArray
¶ Remove specified objects from list.
Signature
RemoveArray(objects)
Parameters: objects (list of NXOpen.Annotations.BaseCustomSymbol
) – Objects to removeReturns: True if succesully removed from list; False if the object was not a member of the list :rtype: bool
New in version NX5.0.0.
License requirements: None.
SetArray¶
-
SelectBaseCustomSymbolList.
SetArray
¶ Overloaded method SetArray
SetArray(objects)
SetArray(vars)
-------------------------------------
Sets the list of objects in the selection list. This will clear any existing items in the list.
Signature
SetArray(objects)
Parameters: objects (list of NXOpen.Annotations.BaseCustomSymbol
) – items to put in the listNew in version NX5.0.0.
License requirements: None.
-------------------------------------
Validate¶
-
SelectBaseCustomSymbolList.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.