InferSnapTypeSnapType Enumeration¶
NXOpen.InferSnapType.SnapType is an alias for NXOpen.InferSnapTypeSnapType
-
class
NXOpen.
InferSnapTypeSnapType
¶ Bases:
object
Specify the snap point type
Enum Members
Enum Member Enum Member Description NotSet No Snap point Start Snap point start End Snap point end Mid Snap point mid Knot Snap point knot Center Snap point center of arc Exist exsisting point Quadrant Snap point quadrant of circle Intersection Snap point intersection Curve Snap point on curve Surf Snap point on surface Origin Snap origin DrfAid Snap point drafting aid DrfTangent Snap point drafting tangent Pole Snap point at pole Defining Snap point at defining ConicAnchor Snap point at conic anchor BoundedGrid Snap point on bounded grid FacetVertex Snap point on facet vertex -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-