RetainedAnnotationsBuilder Class¶
-
class
NXOpen.Annotations.
RetainedAnnotationsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.RetainedAnnotationsBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
LineColorFontWidth | Returns the line color font width of retained drafting objects. |
ShowRetainedAnnotations | Returns or sets the flag indicating to show the retained annotations. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LineColorFontWidth¶
-
RetainedAnnotationsBuilder.
LineColorFontWidth
¶ Returns the line color font width of retained drafting objects.
-------------------------------------
Getter Method
Signature
LineColorFontWidth
Returns: Return type: NXOpen.LineColorFontWidthBuilder
New in version NX9.0.0.
License requirements: None.
ShowRetainedAnnotations¶
-
RetainedAnnotationsBuilder.
ShowRetainedAnnotations
¶ Returns or sets the flag indicating to show the retained annotations.
-------------------------------------
Getter Method
Signature
ShowRetainedAnnotations
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowRetainedAnnotations
Parameters: showRetainedAnnotations (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
RetainedAnnotationsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.