DraftingPointTarget Class¶
-
class
NXOpen.Annotations.
DraftingPointTarget
¶ Bases:
NXOpen.Annotations.DraftingDatumTarget
,NXOpen.Annotations.IPointTarget
Represents drafting point datum target
To create or edit an instance of this class, use
NXOpen.Annotations.DraftingDatumTargetBuilder
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AnnotationOrigin | Returns or sets the origin (location) of the annotation. |
AnnotationPlane | Returns or sets the annotation plane. |
CanChangeLeaderPositionParameter | Returns a flag indicating whether the NXOpen.Annotations.Gdt.LeaderPositionParameter() can be changed |
Color | Returns or sets the color of the object. |
DatumLabel | Returns or sets the datum target label. |
HasAssociativeOrigin | Returns a flag indicating whether the origin is associative |
HasLeaderPositionParameter | Returns a flag indicating whether this GDT has a leader position parameter. |
HasStubbedDatumStyle | Returns or sets a flag indicating whether the leader has a stubbed datum style. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsRetained | Returns a flag indicating whether the annotation is retained |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LeaderOrientation | Returns or sets the leader orientation for the annotation. |
LeaderPositionParameter | Returns or sets a parameter which indicates where the leader end point is located on the object that it is attached to. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
NumberOfAssociativities | Returns the number of associativities for the annotation. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
ParallelToScreen | Returns or sets the PMI parallel to screen setting |
PointCoordinates | Returns the target point coordinates |
Prototype | Returns the prototype of this object if it is an occurrence. |
Suppressed | Returns the flag indicating whether the annotation is suppressed |
Tag | Returns the Tag for this object. |
TargetIndex | Returns or sets the datum target index. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
ConvertToAreaTarget | Converts a datum target point, line, or non-rectangular area to a rectangular area. |
ConvertToDraftingAreaTarget | Converts a drafting datum target point, line, or non-rectangular area to a drafting rectangular area. |
ConvertToDraftingLineTarget | Converts a drafting datum target point or area to a drafting datum target line. |
ConvertToDraftingPointTarget | Converts a drafting datum target line or area to a drafting datum target point. |
ConvertToLineTarget | Converts a datum target point or area to a datum target line. |
ConvertToPointTarget | Converts a datum target line or area to a datum target point. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAssociativeOrigin | Gets data that specifies the origin’s associativity |
GetAssociativity | Returns the associativity at specified index. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetFcfFrameData | Returns the single FCF frames data This is only designed to work with old feature control frames without builders. |
GetFcfFrameDataArray | Returns the multiple FCF frames data This is only designed to work with old feature control frames without builders. |
GetInferredAnnotationPlane | Returns the inferred annotation plane |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLetteringPreferences | Returns the lettering preferences for the annotation |
GetLineAndArrowPreferences | Returns the line and arrow preferences for the annotation |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetSymbolPreferences | Returns the symbol preferences for the annotation |
GetText | Returns the drafting aid’s text |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetUserSymbolPreferences | Returns the user symbol preferences |
GetUserSymbolSize | Gets the user symbol size |
GetViews | Returns the views that the PMI display instance object is displayed in NOTE: This method is only valid for PMI display instance objects. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight | Highlights the object. |
InsertIntoStack | Inserts the annotation into a stack. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveFromStack | Removes the annotation from a stack. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAssociativeOrigin | Associates the annotation’s origin to the specified geometry. |
SetAssociativity | Sets the associativity at specified index. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetFcfFrameData | Sets the single FCF frames data. |
SetLetteringPreferences | Sets the lettering preferences for the annotation. |
SetLineAndArrowPreferences | Sets the line and arrow preferences for the annotation. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSymbolCfw | Sets the symbol color, font, and width. |
SetSymbolPreferences | Sets the symbol preferences for the annotation. |
SetText | Sets the drafting aid’s text. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetUserSymbolPreferences | Sets the user symbol preferences. |
SetUserSymbolSize | Sets the user symbol size. |
SetViews | Sets the views that the PMI display instance object is displayed in. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
DatumLabel¶
-
DraftingPointTarget.
DatumLabel
¶ Returns or sets the datum target label.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
DatumLabel
Returns: Datum label Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumLabel
Parameters: datumLabel (str) – New datum label New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
IsOccurrence¶
-
DraftingPointTarget.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DraftingPointTarget.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
DraftingPointTarget.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
DraftingPointTarget.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DraftingPointTarget.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PointCoordinates¶
-
DraftingPointTarget.
PointCoordinates
¶ Returns the target point coordinates
-------------------------------------
Getter Method
Signature
PointCoordinates
Returns: Point coordinates Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: None.
Prototype¶
-
DraftingPointTarget.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
TargetIndex¶
-
DraftingPointTarget.
TargetIndex
¶ Returns or sets the datum target index.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
TargetIndex
Returns: Datum target index Return type: int New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetIndex
Parameters: index (int) – New datum target index New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
Method Detail¶
FindObject¶
-
DraftingPointTarget.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetFcfFrameData¶
-
DraftingPointTarget.
GetFcfFrameData
¶ Returns the single FCF frames data This is only designed to work with old feature control frames without builders.
For newer feature control frames, the builder should be used to access this data. This method will return an error.
Signature
GetFcfFrameData()
Returns: FCF frame data Return type: NXOpen.Annotations.FcfFrameData
New in version NX4.0.0.
License requirements: None.
GetFcfFrameDataArray¶
-
DraftingPointTarget.
GetFcfFrameDataArray
¶ Returns the multiple FCF frames data This is only designed to work with old feature control frames without builders.
For newer feature control frames, the builder should be used to access this data. This method will return an error.
Signature
GetFcfFrameDataArray()
Returns: FCF frame datas Return type: list of NXOpen.Annotations.FcfFrameData
New in version NX5.0.0.
License requirements: None.
Print¶
-
DraftingPointTarget.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetFcfFrameData¶
-
DraftingPointTarget.
SetFcfFrameData
¶ Overloaded method SetFcfFrameData
SetFcfFrameData(data)
SetFcfFrameData(fcfFrameData)
-------------------------------------
Sets the single FCF frames data. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetFcfFrameData(data)
Parameters: data ( NXOpen.Annotations.FcfFrameData
) – FCF frame dataNew in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
-------------------------------------
Sets the multiple FCF frames data. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetFcfFrameData(fcfFrameData)
Parameters: fcfFrameData (list of NXOpen.Annotations.FcfFrameData
) – FCF frame datasNew in version NX5.0.0.
License requirements: geometric_tol (“GDT”)
-------------------------------------
SetName¶
-
DraftingPointTarget.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.