DatumReference Class¶
-
class
NXOpen.Annotations.
DatumReference
¶ Bases:
NXOpen.TransientObject
Represents a datum reference
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
DatumLabel | Returns or sets the datum label |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetMaterialConditionModifiers | Returns the material condition modifiers |
SetMaterialConditionModifiers | Sets the material condition modifiers |
Property Detail¶
DatumLabel¶
-
DatumReference.
DatumLabel
¶ Returns or sets the datum label
-------------------------------------
Getter Method
Signature
DatumLabel
Returns: Datum label Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumLabel
Parameters: label (str) – New datum label New in version NX4.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
DatumReference.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetMaterialConditionModifiers¶
-
DatumReference.
GetMaterialConditionModifiers
¶ Returns the material condition modifiers
Signature
GetMaterialConditionModifiers()
Returns: List of modifiers Return type: list of NXOpen.Annotations.MaterialConditionModifier
New in version NX4.0.0.
License requirements: None.
SetMaterialConditionModifiers¶
-
DatumReference.
SetMaterialConditionModifiers
¶ Sets the material condition modifiers
Signature
SetMaterialConditionModifiers(modifiers)
Parameters: modifiers (list of NXOpen.Annotations.MaterialConditionModifier
) – List of modifiersNew in version NX4.0.0.
License requirements: None.