MaterialConditionModifier Enumeration¶
-
class
NXOpen.Annotations.
MaterialConditionModifier
¶ Bases:
object
Specifies the material condition modifier Enum Members
Enum Member Enum Member Description Mmc Specifies maximum material condition modifier Lmc Specifies least material condition modifier Rfs Specified regardless of feature size modifier Tangential Specifies tangent plane modifier NotSet Specifies no material modifier. NOTE: This should be used in place of the RFS for ASME 1994 and ISO standards Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-