CircularTargetData Class¶
-
class
NXOpen.Annotations.
CircularTargetData
¶ Bases:
NXOpen.Annotations.DatumTargetData
Represents circular datum target data
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
DatumLabel | Returns or sets the datum label. |
Index | Returns or sets the target index. |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetDiameter | Returns the diameter |
GetSimpleDraftingAidPreferences | Returns the SimpleDraftingAidPreferences object |
SetDiameter | Sets the diameter |
SetSimpleDraftingAidPreferences | Sets the SimpleDraftingAidPreferences object |
Method Detail¶
Dispose¶
-
CircularTargetData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetDiameter¶
-
CircularTargetData.
GetDiameter
¶ Returns the diameter
Signature
GetDiameter()
Returns: Diameter data Return type: NXOpen.Annotations.Value
New in version NX4.0.0.
License requirements: None.
SetDiameter¶
-
CircularTargetData.
SetDiameter
¶ Sets the diameter
Signature
SetDiameter(diameter)
Parameters: diameter ( NXOpen.Annotations.Value
) – New diameter dataNew in version NX4.0.0.
License requirements: None.