DatumTargetData Class¶
-
class
NXOpen.Annotations.
DatumTargetData
¶ Bases:
NXOpen.TransientObject
Represents datum target data
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
DatumLabel | Returns or sets the datum label. |
Index | Returns or sets the target index. |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetSimpleDraftingAidPreferences | Returns the SimpleDraftingAidPreferences object |
SetSimpleDraftingAidPreferences | Sets the SimpleDraftingAidPreferences object |
Property Detail¶
DatumLabel¶
-
DatumTargetData.
DatumLabel
¶ Returns or sets the datum label.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
DatumLabel
Returns: Datum label Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumLabel
Parameters: datumLabel (str) – New datum label New in version NX4.0.0.
License requirements: None.
Index¶
-
DatumTargetData.
Index
¶ Returns or sets the target index.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
Index
Returns: Target index Return type: int New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Index
Parameters: index (int) – New target index New in version NX4.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
DatumTargetData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetSimpleDraftingAidPreferences¶
-
DatumTargetData.
GetSimpleDraftingAidPreferences
¶ Returns the SimpleDraftingAidPreferences object
Signature
GetSimpleDraftingAidPreferences()
Returns: Datum target preferences Return type: NXOpen.Annotations.SimpleDraftingAidPreferences
New in version NX4.0.0.
License requirements: None.
SetSimpleDraftingAidPreferences¶
-
DatumTargetData.
SetSimpleDraftingAidPreferences
¶ Sets the SimpleDraftingAidPreferences object
Signature
SetSimpleDraftingAidPreferences(preferences)
Parameters: preferences ( NXOpen.Annotations.SimpleDraftingAidPreferences
) – New datum target preferencesNew in version NX4.0.0.
License requirements: None.