TypeMappingListBuilder Class¶
-
class
NXOpen.AME.
TypeMappingListBuilder
¶ Bases:
NXOpen.Builder
Type Mapping List Builder
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateTypeMappingListBuilder()
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateTypeMapping | Create a new type mapping |
DeleteTypeMapping | Delete type mapping |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
LoadAd | Loads the Ld types linked to the given AD type |
LoadAllLdTypes | Loads the Ld types in the project |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
List¶
-
TypeMappingListBuilder.
List
¶ Returns the pair list
-------------------------------------
Getter Method
Signature
List
Returns: Return type: NXOpen.AME.TypeMappingBuilderList
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
CreateTypeMapping¶
-
TypeMappingListBuilder.
CreateTypeMapping
¶ Create a new type mapping
Signature
CreateTypeMapping()
Returns: Return type: NXOpen.AME.TypeMappingBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
DeleteTypeMapping¶
-
TypeMappingListBuilder.
DeleteTypeMapping
¶ Delete type mapping
Signature
DeleteTypeMapping(mappingBuilder)
Parameters: mappingBuilder ( NXOpen.AME.TypeMappingBuilder
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
LoadAd¶
-
TypeMappingListBuilder.
LoadAd
¶ Loads the Ld types linked to the given AD type
Signature
LoadAd(adPath)
Parameters: adPath (str) – Returns: Return type: list of NXOpen.AME.TypeMappingBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
LoadAllLdTypes¶
-
TypeMappingListBuilder.
LoadAllLdTypes
¶ Loads the Ld types in the project
Signature
LoadAllLdTypes()
Returns: Return type: list of NXOpen.AME.TypeMappingBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
TypeMappingListBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.