TypeMappingBuilder Class¶
-
class
NXOpen.AME.
TypeMappingBuilder
¶ Bases:
NXOpen.Builder
JA class for the type mapping dialog
this is a block
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AdType | Returns the ad type selection |
LdType | Returns the ld type selection |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Load | Load new type mapping base on part |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdType¶
-
TypeMappingBuilder.
AdType
¶ Returns the ad type selection
-------------------------------------
Getter Method
Signature
AdType
Returns: Return type: NXOpen.Tooling.SelectReuseLibraryItemBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
LdType¶
-
TypeMappingBuilder.
LdType
¶ Returns the ld type selection
-------------------------------------
Getter Method
Signature
LdType
Returns: Return type: NXOpen.Tooling.SelectReuseLibraryItemBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Load¶
-
TypeMappingBuilder.
Load
¶ Load new type mapping base on part
Signature
Load(ldPath)
Parameters: ldPath (str) – Returns: a tuple Return type: A tuple consisting of (adPath, adDescriptiveName) adPath is a str. adDescriptiveName is a str. New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
TypeMappingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.