SelectMountingInterfaceLocationBuilder Class¶
-
class
NXOpen.AME.
SelectMountingInterfaceLocationBuilder
¶ Bases:
NXOpen.Builder
Builder for selecting mounting interface location from graphics window
This object does not need a creator
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
FixingPlacementLocation | Returns or sets the co-ordinate of fixing placement location |
SelectedReceptacleObject | Returns or sets the tag of selected receptacle object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FixingPlacementLocation¶
-
SelectMountingInterfaceLocationBuilder.
FixingPlacementLocation
¶ Returns or sets the co-ordinate of fixing placement location
-------------------------------------
Getter Method
Signature
FixingPlacementLocation
Returns: Return type: NXOpen.Point3d
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
FixingPlacementLocation
Parameters: targetLocation ( NXOpen.Point3d
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SelectedReceptacleObject¶
-
SelectMountingInterfaceLocationBuilder.
SelectedReceptacleObject
¶ Returns or sets the tag of selected receptacle object
-------------------------------------
Getter Method
Signature
SelectedReceptacleObject
Returns: Return type: NXOpen.NXObject
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
SelectedReceptacleObject
Parameters: selectedObjectTag ( NXOpen.NXObject
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
SelectMountingInterfaceLocationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.