QueryBuilder Class¶
-
class
NXOpen.AME.
QueryBuilder
¶ Bases:
NXOpen.Builder
Represents query class builder
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateQueryBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CreationType | Returns or sets the defined rule type |
Description | Returns or sets the query description |
Name | Returns or sets the query name |
Parent | Returns the parent node of query node |
ReuseLibraryItem | Returns the public query |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPublicQueryDescription | The selected public query description |
GetPublicQueryName | The selected public query name |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
QueryBuilderTypes Enumeration | the creation type of query |
Property Detail¶
CreationType¶
-
QueryBuilder.
CreationType
¶ Returns or sets the defined rule type
-------------------------------------
Getter Method
Signature
CreationType
Returns: Return type: NXOpen.AME.QueryBuilderTypes
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
CreationType
Parameters: type ( NXOpen.AME.QueryBuilderTypes
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Description¶
-
QueryBuilder.
Description
¶ Returns or sets the query description
-------------------------------------
Getter Method
Signature
Description
Returns: Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
Description
Parameters: description (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Name¶
-
QueryBuilder.
Name
¶ Returns or sets the query name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Parent¶
-
QueryBuilder.
Parent
¶ Returns the parent node of query node
-------------------------------------
Getter Method
Signature
Parent
Returns: Return type: NXOpen.AME.SelectAMEBaseNode
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ReuseLibraryItem¶
-
QueryBuilder.
ReuseLibraryItem
¶ Returns the public query
-------------------------------------
Getter Method
Signature
ReuseLibraryItem
Returns: Return type: NXOpen.Tooling.SelectReuseLibraryItemBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
GetPublicQueryDescription¶
-
QueryBuilder.
GetPublicQueryDescription
¶ The selected public query description
Signature
GetPublicQueryDescription()
Returns: Return type: str New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetPublicQueryName¶
-
QueryBuilder.
GetPublicQueryName
¶ The selected public query name
Signature
GetPublicQueryName()
Returns: Return type: str New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
QueryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.