QueryBuilderTypes Enumeration¶
NXOpen.AME.QueryBuilder.Types is an alias for NXOpen.AME.QueryBuilderTypes
-
class
NXOpen.AME.
QueryBuilderTypes
¶ Bases:
object
the creation type of query
Enum Members
Enum Member Enum Member Description NewQuery FromLibrary -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-