PortsManagerBuilder Class¶
-
class
NXOpen.AME.
PortsManagerBuilder
¶ Bases:
NXOpen.Builder
Provides journal methods for the ports manager dialog.
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreatePortsManagerBuilder()
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateConnections | Creates the connections |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Disconnect | Disconnects port |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExpression | Gets the dynamic connection expression |
GetObject | Returns the object currently being edited by this builder. |
SetExpression | Sets the dynamic connection expression |
SetPort | Sets the source port of the connection |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateSelection | Updates the IPortsContainer selection |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
CreateConnections¶
-
PortsManagerBuilder.
CreateConnections
¶ Creates the connections
Signature
CreateConnections(source)
Parameters: source ( NXOpen.NXObject
) –Returns: Return type: list of NXOpen.NXObject
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Disconnect¶
-
PortsManagerBuilder.
Disconnect
¶ Disconnects port
Signature
Disconnect(port)
Parameters: port ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetExpression¶
-
PortsManagerBuilder.
GetExpression
¶ Gets the dynamic connection expression
Signature
GetExpression()
Returns: Return type: NXOpen.NXObject
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetExpression¶
-
PortsManagerBuilder.
SetExpression
¶ Sets the dynamic connection expression
Signature
SetExpression(exp)
Parameters: exp ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetPort¶
-
PortsManagerBuilder.
SetPort
¶ Sets the source port of the connection
Signature
SetPort(exp)
Parameters: exp ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
UpdateSelection¶
-
PortsManagerBuilder.
UpdateSelection
¶ Updates the IPortsContainer selection
Signature
UpdateSelection(port)
Parameters: port ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
PortsManagerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.