PageBuilder Class¶
-
class
NXOpen.AME.
PageBuilder
¶ Bases:
NXOpen.AME.EngineeringObjectBaseBuilder
Represents a Page creation class Builder
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreatePageBuilder()
Default values.
Property Value PageName 1 Type MultiLineSchematics New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Aspects | Returns the Page aspect details |
Description | Returns or sets the Page description |
PageAttributeHolder | Returns the attribute holder |
PageName | Returns or sets the Page name |
Tag | Returns the Tag for this object. |
Type | Returns or sets the Page type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedAspects | Get the commited Aspect |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNewObjects | Get the commited Aspect |
GetObject | Returns the object currently being edited by this builder. |
SetClassificationCode | Set user Classification Code. |
SetDefaultClassificationCode | Set default Classification Code. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PageBuilderTypes Enumeration | Represents the type of page |
Property Detail¶
Aspects¶
-
PageBuilder.
Aspects
¶ Returns the Page aspect details
-------------------------------------
Getter Method
Signature
Aspects
Returns: Return type: NXOpen.AME.AspectDetailsBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Description¶
-
PageBuilder.
Description
¶ Returns or sets the Page description
-------------------------------------
Getter Method
Signature
Description
Returns: Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
Description
Parameters: pageDescription (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
PageAttributeHolder¶
-
PageBuilder.
PageAttributeHolder
¶ Returns the attribute holder
-------------------------------------
Getter Method
Signature
PageAttributeHolder
Returns: Return type: NXOpen.AME.PageAttributeHolder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
PageName¶
-
PageBuilder.
PageName
¶ Returns or sets the Page name
-------------------------------------
Getter Method
Signature
PageName
Returns: Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
PageName
Parameters: pageName (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Type¶
-
PageBuilder.
Type
¶ Returns or sets the Page type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.AME.PageBuilderTypes
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.AME.PageBuilderTypes
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
SetClassificationCode¶
-
PageBuilder.
SetClassificationCode
¶ Set user Classification Code.
Signature
SetClassificationCode(dccString)
Parameters: dccString (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetDefaultClassificationCode¶
-
PageBuilder.
SetDefaultClassificationCode
¶ Set default Classification Code.
Signature
SetDefaultClassificationCode()
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
PageBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.