AspectDetailsBuilder Class¶
-
class
NXOpen.AME.
AspectDetailsBuilder
¶ Bases:
NXOpen.Builder
JA Class for the Aspect Details UI Block
This object does not need a creator.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
SelectionParent | Returns the selection parent |
ShowInAutomation | Returns or sets the availability in Automation Navigator |
ShowInFunction | Returns or sets the availability in Function Aspect |
ShowInLocation | Returns or sets the availability in Location Aspect |
ShowInProduct | Returns or sets the availability in Product Aspect |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectionParent¶
-
AspectDetailsBuilder.
SelectionParent
¶ Returns the selection parent
-------------------------------------
Getter Method
Signature
SelectionParent
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowInAutomation¶
-
AspectDetailsBuilder.
ShowInAutomation
¶ Returns or sets the availability in Automation Navigator
-------------------------------------
Getter Method
Signature
ShowInAutomation
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowInAutomation
Parameters: showInAutomation (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowInFunction¶
-
AspectDetailsBuilder.
ShowInFunction
¶ Returns or sets the availability in Function Aspect
-------------------------------------
Getter Method
Signature
ShowInFunction
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowInFunction
Parameters: showInFunction (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowInLocation¶
-
AspectDetailsBuilder.
ShowInLocation
¶ Returns or sets the availability in Location Aspect
-------------------------------------
Getter Method
Signature
ShowInLocation
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowInLocation
Parameters: showInLocation (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowInProduct¶
-
AspectDetailsBuilder.
ShowInProduct
¶ Returns or sets the availability in Product Aspect
-------------------------------------
Getter Method
Signature
ShowInProduct
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowInProduct
Parameters: showInProduct (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
AspectDetailsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.