ObjectConnectionDetailBuilder Class¶
-
class
NXOpen.AME.
ObjectConnectionDetailBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
JA class for the reuse object connection detail block
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
PropertyString | Returns or sets the selected property name |
ResultString | Returns the result string text |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ChangeEditObject | Change the edit object |
Populate | Populate selection |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
PropertyString¶
-
ObjectConnectionDetailBuilder.
PropertyString
¶ Returns or sets the selected property name
-------------------------------------
Getter Method
Signature
PropertyString
Returns: Return type: str New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
PropertyString
Parameters: propertyName (str) – New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
ChangeEditObject¶
-
ObjectConnectionDetailBuilder.
ChangeEditObject
¶ Change the edit object
Signature
ChangeEditObject(newObject)
Parameters: newObject ( NXOpen.NXObject
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Populate¶
-
ObjectConnectionDetailBuilder.
Populate
¶ Populate selection
Signature
Populate(hierarchy)
Parameters: hierarchy (list of str) – New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
ObjectConnectionDetailBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.