MapToExistingObjectBuilder Class¶
-
class
NXOpen.AME.
MapToExistingObjectBuilder
¶ Bases:
NXOpen.Builder
Line Designer map to existing (EO) dialog JA interface
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateMapToExistingObjectBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
MapTemplateToggle | Returns or sets the toggle whether to map to template |
SelectionAD | Returns the get selectionAD |
SelectionLD | Returns the get selectionLD |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InsertIntoSelectionAD | The insert into selectionAD |
InsertIntoSelectionLD | The insert into selectionAD |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
MapTemplateToggle¶
-
MapToExistingObjectBuilder.
MapTemplateToggle
¶ Returns or sets the toggle whether to map to template
-------------------------------------
Getter Method
Signature
MapTemplateToggle
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
MapTemplateToggle
Parameters: mapTemplateToggle (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SelectionAD¶
-
MapToExistingObjectBuilder.
SelectionAD
¶ Returns the get selectionAD
-------------------------------------
Getter Method
Signature
SelectionAD
Returns: Return type: NXOpen.AME.SelectAMEBaseNodeList
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SelectionLD¶
-
MapToExistingObjectBuilder.
SelectionLD
¶ Returns the get selectionLD
-------------------------------------
Getter Method
Signature
SelectionLD
Returns: Return type: NXOpen.SelectNXObject
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
InsertIntoSelectionAD¶
-
MapToExistingObjectBuilder.
InsertIntoSelectionAD
¶ The insert into selectionAD
Signature
InsertIntoSelectionAD(adObject)
Parameters: adObject ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
InsertIntoSelectionLD¶
-
MapToExistingObjectBuilder.
InsertIntoSelectionLD
¶ The insert into selectionAD
Signature
InsertIntoSelectionLD(ldObject)
Parameters: ldObject ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
MapToExistingObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.