LineDesignerMappingBuilder Class¶
-
class
NXOpen.AME.
LineDesignerMappingBuilder
¶ Bases:
NXOpen.Builder
Line Designer mapping dialog JA interface
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateLineDesignerMappingBuilder()
Default values.
Property Value EnumFilter Unhidden New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
EnumFilter | Returns or sets the enum filter |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateEngineeringObjectAndMap | Creates a new automation designer object and maps it to a line designer object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Hide | Hide a ld object |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Unhide | Unhide a ld object |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LineDesignerMappingBuilderFilterType Enumeration | enum for the filter |
Property Detail¶
EnumFilter¶
-
LineDesignerMappingBuilder.
EnumFilter
¶ Returns or sets the enum filter
-------------------------------------
Getter Method
Signature
EnumFilter
Returns: Return type: NXOpen.AME.LineDesignerMappingBuilderFilterType
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
EnumFilter
Parameters: enumFilter ( NXOpen.AME.LineDesignerMappingBuilderFilterType
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
CreateEngineeringObjectAndMap¶
-
LineDesignerMappingBuilder.
CreateEngineeringObjectAndMap
¶ Overloaded method CreateEngineeringObjectAndMap
CreateEngineeringObjectAndMap(ldObject)
CreateEngineeringObjectAndMap(ldObjects)
-------------------------------------
Creates a new automation designer object and maps it to a line designer object.
Signature
CreateEngineeringObjectAndMap(ldObject)
Parameters: ldObject ( NXOpen.NXObject
) –Returns: Return type: NXOpen.NXObject
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Creates new automation designer objects and maps them to line designer objects in bulk.
Signature
CreateEngineeringObjectAndMap(ldObjects)
Parameters: ldObjects (list of NXOpen.NXObject
) – Line designer objects to mapReturns: Mapped automation designer objects Return type: list of NXOpen.NXObject
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Hide¶
-
LineDesignerMappingBuilder.
Hide
¶ Hide a ld object
Signature
Hide(ldObject)
Parameters: ldObject ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Unhide¶
-
LineDesignerMappingBuilder.
Unhide
¶ Unhide a ld object
Signature
Unhide(ldObject)
Parameters: ldObject ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
LineDesignerMappingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.