CreateTemplateBuilder Class¶
-
class
NXOpen.AME.
CreateTemplateBuilder
¶ Bases:
NXOpen.Builder
Create Template dialog JA class
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateTemplateBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CreateFragmentToggle | Returns or sets the template toggle for create fragment |
SelectedObjects | Returns the selected objects from project |
Tag | Returns the Tag for this object. |
TemplateNameAndDescription | Returns the template name and description ui block |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateTemplateProject | Creates the template project |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateFragmentToggle¶
-
CreateTemplateBuilder.
CreateFragmentToggle
¶ Returns or sets the template toggle for create fragment
-------------------------------------
Getter Method
Signature
CreateFragmentToggle
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
CreateFragmentToggle
Parameters: createFragmentToggle (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SelectedObjects¶
-
CreateTemplateBuilder.
SelectedObjects
¶ Returns the selected objects from project
-------------------------------------
Getter Method
Signature
SelectedObjects
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
TemplateNameAndDescription¶
-
CreateTemplateBuilder.
TemplateNameAndDescription
¶ Returns the template name and description ui block
-------------------------------------
Getter Method
Signature
TemplateNameAndDescription
Returns: Return type: NXOpen.AME.ObjectNameBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
CreateTemplateProject¶
-
CreateTemplateBuilder.
CreateTemplateProject
¶ Creates the template project
Signature
CreateTemplateProject()
Returns: Return type: NXOpen.AME.Project
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
CreateTemplateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.