ObjectNameBuilder Class¶
-
class
NXOpen.AME.
ObjectNameBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Object Name JA class
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ObjectDescription | Returns or sets the object description |
ObjectName | Returns or sets the object name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GenerateName | Geneate a new unique name |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ObjectDescription¶
-
ObjectNameBuilder.
ObjectDescription
¶ Returns or sets the object description
-------------------------------------
Getter Method
Signature
ObjectDescription
Returns: Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ObjectDescription
Parameters: objectDescription (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ObjectName¶
-
ObjectNameBuilder.
ObjectName
¶ Returns or sets the object name
-------------------------------------
Getter Method
Signature
ObjectName
Returns: Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ObjectName
Parameters: objectName (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
GenerateName¶
-
ObjectNameBuilder.
GenerateName
¶ Geneate a new unique name
Signature
GenerateName(baseName)
Parameters: baseName (str) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
ObjectNameBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.