CreateProductBuilder Class¶
-
class
NXOpen.AME.
CreateProductBuilder
¶ Bases:
NXOpen.Builder
Create and classify product
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateProductBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
SelectClassificationFromTree | Returns the select classification from tree builder. |
SelectionEngObjectDefinition | Returns the engineering object definition |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateTypeAttribute | Creates a new type attribute object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetObjectNameOnTypeAttr | Sets the Object Name on Type Attribute Object. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectClassificationFromTree¶
-
CreateProductBuilder.
SelectClassificationFromTree
¶ Returns the select classification from tree builder.
-------------------------------------
Getter Method
Signature
SelectClassificationFromTree
Returns: Return type: NXOpen.AME.SelectClassificationFromTreeBuilder
New in version NX11.0.0.
Deprecated since version NX12.0.0: The newly created product is placed under the product library node which corresponds to the Type Library path of the selected Device Type. If the selected type has no counterpart in the Product structure, system automatically places those directly under Device Product Library node.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SelectionEngObjectDefinition¶
-
CreateProductBuilder.
SelectionEngObjectDefinition
¶ Returns the engineering object definition
-------------------------------------
Getter Method
Signature
SelectionEngObjectDefinition
Returns: Return type: NXOpen.AME.SelectionEngineeringObjectDefinitionBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
CreateTypeAttribute¶
-
CreateProductBuilder.
CreateTypeAttribute
¶ Creates a new type attribute object
Signature
CreateTypeAttribute()
Returns: Return type: NXOpen.NXObject
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetObjectNameOnTypeAttr¶
-
CreateProductBuilder.
SetObjectNameOnTypeAttr
¶ Sets the Object Name on Type Attribute Object.
Signature
SetObjectNameOnTypeAttr()
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
CreateProductBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.