ConfigureResultTableBuilder Class¶
-
class
NXOpen.AME.
ConfigureResultTableBuilder
¶ Bases:
NXOpen.Builder
Represents configure result table class builder
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateConfigureResultTableBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
SelectedClassification | Returns the selected classification |
SourceObject | Returns the source object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Add | The action to add properties |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
MoveDown | The action to move added column down |
MoveUp | The action to move added column up |
Remove | The action to move earlier added column |
SetVisibility | The visibility status of each column or group |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectedClassification¶
-
ConfigureResultTableBuilder.
SelectedClassification
¶ Returns the selected classification
-------------------------------------
Getter Method
Signature
SelectedClassification
Returns: Return type: NXOpen.AME.SelectClassificationBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SourceObject¶
-
ConfigureResultTableBuilder.
SourceObject
¶ Returns the source object
-------------------------------------
Getter Method
Signature
SourceObject
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Add¶
-
ConfigureResultTableBuilder.
Add
¶ The action to add properties
Signature
Add(groupName, propertyName)
Parameters: - groupName (str) –
- propertyName (str) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
MoveDown¶
-
ConfigureResultTableBuilder.
MoveDown
¶ The action to move added column down
Signature
MoveDown(groupName, propertyName)
Parameters: - groupName (str) –
- propertyName (str) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
MoveUp¶
-
ConfigureResultTableBuilder.
MoveUp
¶ The action to move added column up
Signature
MoveUp(groupName, propertyName)
Parameters: - groupName (str) –
- propertyName (str) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Remove¶
-
ConfigureResultTableBuilder.
Remove
¶ The action to move earlier added column
Signature
Remove(groupName, propertyName)
Parameters: - groupName (str) –
- propertyName (str) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetVisibility¶
-
ConfigureResultTableBuilder.
SetVisibility
¶ The visibility status of each column or group
Signature
SetVisibility(groupName, propertyName, visibility)
Parameters: - groupName (str) –
- propertyName (str) –
- visibility (bool) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
ConfigureResultTableBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.