SelectClassificationBuilder Class¶
-
class
NXOpen.AME.
SelectClassificationBuilder
¶ Bases:
NXOpen.Tooling.SelectReuseLibraryItemBuilder
Select a part from the reuse library
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ClassName | Returns or sets the class of the name from the reuse library classification |
DescriptiveName | Returns or sets the descriptive name |
Selection | Returns or sets the path of the file from the reuse library |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
ClassName¶
-
SelectClassificationBuilder.
ClassName
¶ Returns or sets the class of the name from the reuse library classification
-------------------------------------
Getter Method
Signature
ClassName
Returns: the class of a name Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ClassName
Parameters: path (str) – the class of a name New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)