Changes the current directory.
Lists the contents of the current directory. You can specify a file template.
Changes current listing device. Output from compile and link commands are directed to the specified device. Enter the corresponding value for the desired device as follows: (Also see &LDEV .)
1) SCREEN (CRT)
2) LINE PRINTER (LP)
3) FILE
4) SUPPRESS OUTPUT (NULL)
Toggles compiler listing mode between All and Errors Only. The All option produces a listing which consists of GRIP source statements, variable storage locations, labels, array sizes, and errors. Errors Only produces a listing which consists of only compilation errors.
Allows you to specify a different editor (for example, vi) as the current editor.