&LDEV
Allows access to the current listing device specified. An integer will be returned to a receiving variable representing the current device. The current device can also be assigned; however, the only valid assignments are 1 (CRT), 2 (line printer), 6 (CRT and line printer), and 10 (no output).
Read/Write - Number - [1..10]
1 = &CRT
2 = &LPT
6 = CRT and Line Printer
10 = Null
Parameter |
Description |
&CRT |
GPA which indicates that the current listing device is the CRT. |
&LPT |
GPA which indicates that the current listing device is the system line printer. |
CRT and Line Printer |
Indicates that the current listing device will be the CRT and the system line printer. |
Null |
Indicates that output will be suppressed. |