/*
uf_assem_types.h
****************************************************************************/
#ifndef UF_ASSEM_TYPES_INCLUDED
#define UF_ASSEM_TYPES_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_fam_types.h>
#define UF_ASSEM_load_from_directory 0
#define UF_ASSEM_load_from_search_dirs 1
#define UF_ASSEM_load_as_saved 2
#define UF_ASSEM_managed_load_by_revision_rule 1
#define UF_ASSEM_managed_load_as_saved 2
#define UF_ASSEM_do_not_add_components 0
#define UF_ASSEM_add_single_level 1
#define UF_ASSEM_add_all_levels 2
#define UF_ASSEM_no_update_report 1
#define UF_ASSEM_update_report 2
#define UF_ASSEM_do_not_emphasize_wp 1
#define UF_ASSEM_emphasize_wp 2
#define UF_ASSEM_do_abort_on_failure 0
#define UF_ASSEM_dont_abort_on_failure 1
#define UF_ASSEM_dont_maintain_work_part 0
#define UF_ASSEM_do_maintain_work_part 1
#define UF_ASSEM_load_exact_version 0
#define UF_ASSEM_load_latest_version 1
#define UF_ASSEM_dont_load_components 0
#define UF_ASSEM_do_load_components 1
#define UF_ASSEM_use_last_component_set 2
#define UF_ASSEM_specify_filter 4 /*This option is only valid for internal programs. */
/*
New options for v10.4. For earlier versions, the default behaviour
was 0 (load components partially)
*/
#define UF_ASSEM_load_components_partially 0
#define UF_ASSEM_load_components_fully 1
/*
New options for NX7.5 to determine whether lightweight representations is on or off.
The default behavior is 0 i.e. don't allow lightweight representations
*/
#define UF_ASSEM_do_allow_lightweight_representations 1
#define UF_ASSEM_dont_allow_lightweight_representations 0
/*
New option for auto regenerating missing part family members during
the load of the assembly. The default behaviour is 1 i.e. to auto
regenerate the missing part family members
*/
#define UF_ASSEM_dont_auto_generate_pfm 0
#define UF_ASSEM_auto_generate_pfm 1
#define UF_ASSEM_dont_allow_substitution 0
#define UF_ASSEM_do_allow_substitution 1
#define UF_ASSEM_dont_apply_to_all_levels 0
#define UF_ASSEM_do_apply_to_all_levels 1
/*
New option for V14.0, load WAVE data, comes into effect if partial loading
is enabled.
UF_ASSEM_default_load_behaviour - No special processing of Wave data
or parents
UF_ASSEM_load_wave_data - Load weave data and parents as
controlled by load_wave_parents
UF_ASSEM_none - Don't load unlaoded parents, but
ensure partially loaded parents
are fully loaded
UF_ASSEM_immediate - Load immediate parents of any WAVE
data
UF_ASSEM_all - Load parents of WAVE data, and
parents of that, until no parents
can be found
*/
#define UF_ASSEM_default_load_behaviour 0
#define UF_ASSEM_load_wave_data 1
#define UF_ASSEM_none 0
#define UF_ASSEM_immediate 1
#define UF_ASSEM_all 2
/***************************************************************
* History:
* NX2: parts_list is no longer used.
* NX8.5: managed_mode_load_options introduced.
***************************************************************/
struct UF_ASSEM_options_s
{
int load_options; /* Load Options - for native mode only
UF_ASSEM_load_from_directory
UF_ASSEM_load_from_search_dirs
UF_ASSEM_load_as_saved
*/
int parts_list; /* NOTE: parts_list is no longer used */
int update; /*Update report setting -
UF_ASSEM_no_update_report
UF_ASSEM_update_report
*/
int emphasize; /*Emphasize setting -
UF_ASSEM_do_not_emphasize_wp
UF_ASSEM_emphasize_wp
*/
int emphasize_color; /* NOTE: emphasize_color is no longer used */
int failure_action; /* failure Option value -
UF_ASSEM_do_abort_on_failure
UF_ASSEM_dont_abort_on_failure
*/
int maintain_work_part; /* Option to apply to the work part when
changing the displayed part interactively:
UF_ASSEM_dont_maintain_work_part
Work part set to be displayed part after
a Change Displayed Part operation.
UF_ASSEM_do_maintain_work_part
Work part unchanged after a Change
Displayed Part operation, provided that
the work part is under the new displayed
part, and has the same units as the new
displayed part.
*/
int load_latest; /* Load latest version switch
UF_ASSEM_load_exact_version
UF_ASSEM_load_latest_version
*/
int load_components; /* Load components option
UF_ASSEM_dont_load_components
UF_ASSEM_do_load_components
UF_ASSEM_use_last_component_set
UF_ASSEM_use_last_filter
UF_ASSEM_specify_filter
*/
int load_fully; /* Full load switch
UF_ASSEM_load_components_partially
UF_ASSEM_load_components_fully
*/
int use_lightweight_representations; /* Lightweight Representations option
UF_ASSEM_do_allow_lightweight_representations
UF_ASSEM_dont_allow_lightweight_representations
*/
int load_substitution; /* Allow Substitution switch
UF_ASSEM_dont_allow_substitution
UF_ASSEM_do_allow_substitution
*/
int apply_to_all_levels; /* Apply reference set defaults to all levels
UF_ASSEM_dont_apply_to_all_levels
UF_ASSEM_do_apply_to_all_levels
prior to V13, the behavior was
UF_ASSEM_dont_apply_to_all_levels.
*/
int load_wave_data; /* New option for V14, if load_fully is set to
UF_ASSEM_load_components_partially then
this allows for components with WAVE data
in them to be fully loaded. Other components
will still be partially loaded.
UF_ASSEM_default_load_behaviour
UF_ASSEM_load_wave_data
*/
int load_wave_parents; /* Load Unloaded Wave Parents option. This
field is only used if load_wave_data is set
to UF_ASSEM_load_wave_data. When it is, this
value controls the way in which parents of
wave geometry are loaded:
UF_ASSEM_none - Don't load unloaded parents,
but ensure partially loaded
parents are fully loaded.
UF_ASSEM_immediate - Load immediate parents
of any WAVE data.
UF_ASSEM_all - Load parents of WAVE data,
and their parents, until no
parents can be found.
A parent part is one which contains geometry
that is linked to another part. If part A
has a LINKED_BODY which references geometry
in part B, then set the load options as
follows:
load_wave_data = UF_ASSEM_load_wave_data
load_wave_parents = UF_ASSEM_immediate
If you load part A, then part B is loaded.
*/
int auto_regen_pfm_option; /* Auto regenerate missing part family children
option. If this option is set to
UF_ASSEM_auto_generate_pfm then while loading
assemblies, any missing part family members
will be automatically regenerated.
The valid options are:
UF_ASSEM_auto_generate_pfm
UF_ASSEM_dont_auto_generate_pfm
*/
int managed_mode_load_options; /* Load Options - for managed mode only
UF_ASSEM_managed_load_by_revision_rule
UF_ASSEM_managed_load_as_saved
*/
};
typedef struct UF_ASSEM_options_s UF_ASSEM_options_t, *UF_ASSEM_options_p_t;
/*
Assembly Upgrade status structure
*/
struct UF_ASSEM_upgrade_status_s
{
logical failed; /* true if any components could not be upgraded */
int n_components; /* length of the following two arrays */
char **component_names; /* array of component names that failed to upgrade.
This array must be freed using
UF_free_string_array.
*/
int *statuses; /* associated statuses with each file name. This
array must be freed using UF_free. */
};
typedef struct UF_ASSEM_upgrade_status_s UF_ASSEM_upgrade_status_t,
*UF_ASSEM_upgrade_status_p_t;
/******************************************************************************
Component array functions.
There are two types of component arrays - those which are based on feature
instance sets (iset arrays) and those which are based on a master component
(mc arrays).
Each type of array has a data structure which defines the contents of the
array. These structures are used as arguments to the various array functions.
******************************************************************************/
/* These constants are used for the array_subtype field.
*/
#define UF_ASSEM_iset_array 1
#define UF_ASSEM_linear_array 2
#define UF_ASSEM_circular_array 3
/* This defines the maximum number of dimensions for a component array.
This is currently 2 (X and Y)
*/
#define UF_ASSEM_max_dim_count 2
/*
Component array based on a master component. Also referred to as an
mc array.
*/
struct UF_ASSEM_mc_array_data_s
{
int array_subtype; /* A flag indicating which type of array this is.
It will either be UF_ASSEM_linear_array or
UF_ASSEM_circular_array . */
tag_t master_component; /* The tag of the master component for this
array*/
tag_t template_component; /* The tag of the template component for this
array. */
tag_t dimensions[UF_ASSEM_max_dim_count]; /* An array of expression tags
which determine the size of the array. For
linear arrays, the first element is the
number of components in the X direction, and
the second element is the number of
components in the Y direction. For one
dimensional linear arrays, the second
element will be NULL. For circular arrays,
the second element will be NULL. */
tag_t axis_definitions[UF_ASSEM_max_dim_count]; /* The solid entities
(faces, datums, etc) which determine the
direction of the array. For linear arrays,
the first element defines the X direction,
and the second the Y direction. For one
dimensional linear arrays, the second element
will be NULL. For circular arrays, the first
element is the central axis, and the second
is NULL. If these solid objects are in
component part files, you should pass in
their occurrences in the assembly that
contains the array.*/
tag_t offsets[UF_ASSEM_max_dim_count]; /* An array of expression tags
which determine the spacing between array
elements. For linear arrays, the first
element is the X offset, and the second is
the Y offset. For one dimensional linear
arrays, the second element will be NULL.
For circular arrays, the first element is
the angle between components, and the
second is NULL. */
char *array_name; /* The name of the array object. When this value
is returned from an enquiry function, it is
dynamically allocated, and must be freed with
UF_free. */
};
typedef struct UF_ASSEM_mc_array_data_s UF_ASSEM_mc_array_data_t,
*UF_ASSEM_mc_array_data_p_t;
/*
Component array based on a feature instance-set component. Also referred
to as an iset array.
*/
struct UF_ASSEM_iset_array_data_s
{
tag_t feature_iset; /* The tag of the feature iset that the array
is based upon. Information about the iset
may be obtained by calling
UF_MODL_ask_linear_iset_parms or
UF_MODL_ask_circular_iset_parms as
appropriate. */
tag_t template_component; /* The tag of the template component for this
array. */
int dimensions[UF_ASSEM_max_dim_count]; /* An array of integers which
indicates the size of the array. A referenced iset can
be Linear or Circular. For a linear iset, the first
array element is the number of components in the X direction
and the second element is the number of components
in the Y direction. For a one dimensional linear iset, the
second element will be NULL. For circular arrays, the second
element will be NULL. The dimensions array can be left
unpopulated (or not required) during creation. */
char *array_name; /* The name of the array object. When this
value is returned from an enquiry function,
it is dynamically allocated, and must be
freed by calling UF_free. */
} ;
typedef struct UF_ASSEM_iset_array_data_s UF_ASSEM_iset_array_data_t,
*UF_ASSEM_iset_array_data_p_t;
/******************************************************************************
Instance intent data types.
******************************************************************************/
struct UF_ASSEM_instance_intent_s
{
UF_FAM_intent_data_p_t fam_intent; /* Part family intent. NULL
if no intent exists. */
} ;
typedef struct UF_ASSEM_instance_intent_s UF_ASSEM_instance_intent_t,
*UF_ASSEM_instance_intent_p_t;
struct UF_ASSEM_instance_status_s
{
logical child_changed; /* A flag indicating whether
the child of the instance
has changed. */
tag_t current_child; /* Current child of the
instance. */
tag_t previous_child; /* Previous child of the
instance. */
char *info; /* Additional information.
This can be NULL. */
};
typedef struct UF_ASSEM_instance_status_s UF_ASSEM_instance_status_t,
*UF_ASSEM_instance_status_p_t;
/********************************************************************
* UF_ASSEM_level_option_t is used to control the results of an operation
* to modify a part occurrence, when the part occurrence chosen
* cannot be modified directly for some reason. It is currently
* used for reposition.
*
********************************************************************/
enum UF_ASSEM_level_option_e
{
UF_ASSEM_use_strict_level, /* If the given part occurrence can't be
modified, the operation will fail and return
UF_ASSEM_err_operation_requires_override */
UF_ASSEM_use_existing_level, /* If the given part occurrence can't be
modified, the operation will instead transform
the corresponding part occurrence at the
nearest level down in the assembly where an
appropriate override exists. If none exists
then the instance will be modified. */
UF_ASSEM_establish_override /* If the given part occurrence can't be
modified, the operation will create an override
in the part of the given part occurrence and
then perform the transform. */
};
typedef enum UF_ASSEM_level_option_e UF_ASSEM_level_option_t;
/********************************************************************
* UF_ASSEM_prev16_align_t describes a PreV16 Align constraint which needs to
* be converted to a Distance constraint because its offset direction is
* not interpreted correctly.
*
* This type is used as arguments by the following functions:
* UF_ASSEM_find_prev16_aligns_to_check
* UF_ASSEM_convert_prev16_aligns
* UF_ASSEM_free_prev16_aligns
*
********************************************************************/
struct UF_ASSEM_prev16_align_s
{
tag_t part; /* The part in which the constraint resides */
tag_t condition_tag; /* The mating condition in which the constraint resides */
char *condition_name; /* The name of the mating condition */
int constraint_index; /* The index of the constraint within the mating condition */
char *constraint_name; /* The name of the constraint */
tag_t offset; /* The offset distance expression */
char *offset_name; /* The name of the offset distance expression of the constraint */
double offset_value; /* The value of the offset distance expression of the constraint */
char *message; /* A message indicating any problems related to the conversion of the constraint (might be NULL) */
char *reason; /* A reason explaining the above message (might be NULL) */
};
typedef struct UF_ASSEM_prev16_align_s UF_ASSEM_prev16_align_t, *UF_ASSEM_prev16_align_p_t;
/*
Return value of user registered animation callback function.
*/
#define UF_ASSEM_anim_continue (0) /*If user want to continue to play next frame.*/
#define UF_ASSEM_anim_stop (1) /*If user want to stop current sequence playback.*/
/*
Definition of a callback function mechanism for animation playback.
This callback function will called each frame when user use synchronous play.
*/
typedef int (*UF_ASSEM_animation_callback_f_t)(
void* user_data /* <I> This is a user supplied pointer. */
);
/*********************************************************************/
/* Data returned by
UF_ASSEM_set_work_part_context_quietly
*/
typedef struct UF_ASSEM_work_part_context_s *UF_ASSEM_work_part_context_p_t;
/*********************************************************************/
#endif /* UF_ASSEM_TYPES_INCLUDED */