Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.userdefinedtemplate |
Provides classes and interfaces for User Defined Template.
|
Class and Description |
---|
Collection
Represents a collection of user defined template
To obtain an instance of this class, refer to Part Created in NX10.0.0 |
Class and Description |
---|
Instantiation
Represents an User Defined Template Instantiation object
To create or edit an instance of this class, use InstantiationBuilder Created in NX10.0.0 |
InstantiationBuilder
Represents a
InstantiationBuilder
To create a new instance of this class, use Collection.createInstantiationBuilder(nxopen.userdefinedtemplate.Instantiation) Created in NX10.0.0 |
InstantiationBuilder.JaUserdefinedtemplateLayerOption
Output layer options
|
InstantiationBuilder.MatchedExpressionData
This class holds the data returned from
InstantiationBuilder.getMatchedExpression(nxopen.Expression) |
InstantiationBuilder.MatchedReferenceData
This class holds the data returned from
InstantiationBuilder.getMatchedReference(nxopen.NXObject) |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.