See: Description
Interface | Description |
---|---|
UserDefinedClass |
JA interface for the UserDefinedClass object
To create a new instance of this class, use UserDefinedClassManager.newUserDefinedClass() Created in NX5.0.0 |
UserDefinedClass.DisplayCallback |
Prototype for display, selection, attention point, fit and screen-size-fit callbacks
|
UserDefinedClass.GenericCallback |
Prototype for information, edit, and suppress callbacks
|
UserDefinedClass.LinkCallback |
Prototype for update, and delete callbacks
|
UserDefinedClassManager |
JA interface for the UserDefinedClassManager object
To obtain an instance of this class, refer to Session Created in NX5.0.0 |
UserDefinedDisplayEvent |
Implements the Display Event Object for UDO's .
|
UserDefinedEvent |
Implements the Event Object for UDO's .
|
UserDefinedLinkEvent |
Implements the Display Event Object for UDO's .
|
UserDefinedObject |
JA interface for the UserDefinedObject object .
|
UserDefinedObjectDisplayContext |
This class is used to display User Defined Objects .
|
UserDefinedObjectManager |
This class creates and manages UserDefinedObjects
To obtain an instance of this class, refer to BasePart Created in NX5.0.0 |
Class | Description |
---|---|
UserDefinedClass.AllowOwnedObjectSelection |
Allow owned object selection on all objects owned by an object of this
UserDefinedClass . |
UserDefinedClass.AllowQueryClass |
Allow query class from name options for a
UserDefinedObject of this class. |
UserDefinedClass.Selection |
Allow query class from name options for a
UserDefinedObject . |
UserDefinedEvent.Reason |
Available link types for a
UserDefinedObject . |
UserDefinedObject.LinkDefinition |
Contains the linked object and it's status along with the type of link.
|
UserDefinedObject.LinkStatus |
Status of the object linked to a
UserDefinedObjectFeature |
UserDefinedObject.LinkType |
Available link types for a
UserDefinedObjectFeature . |
UserDefinedObjectDisplayContext.FacetType |
The enumerated type facet to be displayed
|
UserDefinedObjectDisplayContext.PolyMarker |
This enumerated type specifies the type of marker to be displayed.
|
UserDefinedObjectDisplayContext.StandardTextRef |
This enumerated type specifies the type of reference point used in the text box
for standard_text methods.
|
UserDefinedObjectDisplayContext.TextRef |
This enumerated type specifies the type of reference point used in the text box.
|
UserDefinedObjectDisplayContext.TextSize |
Provides a way to specify the size of the desired text, as small,
medium or large (normal is a synonym for medium).
|
UserDefinedObjectDisplayContext.ViewMode |
The enumerated view mode
|
UserDefinedObjectDisplayContext.ViewModeData |
This class holds the data returned from
UserDefinedObjectDisplayContext.getViewMode() |
UserDefinedObjectManager.LinkedUdoDefinition |
Used to define a link to a UserDefinedObject
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.