public static class WireHoleBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SELECT_EDGE |
static int |
_SPECIFY_POINT |
static WireHoleBuilder.Types |
SELECT_EDGE |
static WireHoleBuilder.Types |
SPECIFY_POINT |
Modifier and Type | Method and Description |
---|---|
static WireHoleBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WireHoleBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WireHoleBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final WireHoleBuilder.Types SPECIFY_POINT
public static final WireHoleBuilder.Types SELECT_EDGE
public static final int _SPECIFY_POINT
public static final int _SELECT_EDGE
public static WireHoleBuilder.Types valueOf(int value)
public static WireHoleBuilder.Types valueOf(String name)
public static WireHoleBuilder.Types[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.