public static class StripLayoutStationInformationBuilder.StationItem extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE
Define station number -- 01
|
static int |
_THREE
Define station number -- 03
|
static int |
_TWO
Define station number -- 02
|
static StripLayoutStationInformationBuilder.StationItem |
ONE
Define station number -- 01
|
static StripLayoutStationInformationBuilder.StationItem |
THREE
Define station number -- 03
|
static StripLayoutStationInformationBuilder.StationItem |
TWO
Define station number -- 02
|
Modifier and Type | Method and Description |
---|---|
static StripLayoutStationInformationBuilder.StationItem |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StripLayoutStationInformationBuilder.StationItem |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StripLayoutStationInformationBuilder.StationItem[] |
values()
Returns an array that contains the values for this enum.
|
public static final StripLayoutStationInformationBuilder.StationItem ONE
public static final StripLayoutStationInformationBuilder.StationItem TWO
public static final StripLayoutStationInformationBuilder.StationItem THREE
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static StripLayoutStationInformationBuilder.StationItem valueOf(int value)
public static StripLayoutStationInformationBuilder.StationItem valueOf(String name)
public static StripLayoutStationInformationBuilder.StationItem[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.