public static class StripLayoutBuilder.FromStationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE
the beginning layout station is 1
|
static int |
_THREE
the beginning layout station is 3
|
static int |
_TWO
the beginning layout station is 2
|
static StripLayoutBuilder.FromStationType |
ONE
the beginning layout station is 1
|
static StripLayoutBuilder.FromStationType |
THREE
the beginning layout station is 3
|
static StripLayoutBuilder.FromStationType |
TWO
the beginning layout station is 2
|
Modifier and Type | Method and Description |
---|---|
static StripLayoutBuilder.FromStationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StripLayoutBuilder.FromStationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StripLayoutBuilder.FromStationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final StripLayoutBuilder.FromStationType ONE
public static final StripLayoutBuilder.FromStationType TWO
public static final StripLayoutBuilder.FromStationType THREE
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static StripLayoutBuilder.FromStationType valueOf(int value)
public static StripLayoutBuilder.FromStationType valueOf(String name)
public static StripLayoutBuilder.FromStationType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.