public static class SpreadsheetData.ParameterStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FORCE_COLOR
If the parameter uses user value, normally it shows in UI in a different color.
|
static int |
_HIDDEN_VALUE
The parameter has value, but it should be hidden to user
|
static int |
_HIDE_STATUS
Not shown in UI
|
static int |
_LOCK
User can't change the value in UI
|
static int |
_MODIFIED
The parameter value is changed
|
static int |
_OPTION_VALUE
The parameter has multiple value, but not treated as key parameter
|
static int |
_READ_ONLY
This parameter is read only
|
static int |
_SCALE_ITEM
This is a scale item
|
static int |
_SYSTEM_KEY
This is system key parameter
|
static int |
_USER_KEY
Key parameter analyzed from spreadsheet search
|
static SpreadsheetData.ParameterStatus |
FORCE_COLOR
If the parameter uses user value, normally it shows in UI in a different color.
|
static SpreadsheetData.ParameterStatus |
HIDDEN_VALUE
The parameter has value, but it should be hidden to user
|
static SpreadsheetData.ParameterStatus |
HIDE_STATUS
Not shown in UI
|
static SpreadsheetData.ParameterStatus |
LOCK
User can't change the value in UI
|
static SpreadsheetData.ParameterStatus |
MODIFIED
The parameter value is changed
|
static SpreadsheetData.ParameterStatus |
OPTION_VALUE
The parameter has multiple value, but not treated as key parameter
|
static SpreadsheetData.ParameterStatus |
READ_ONLY
This parameter is read only
|
static SpreadsheetData.ParameterStatus |
SCALE_ITEM
This is a scale item
|
static SpreadsheetData.ParameterStatus |
SYSTEM_KEY
This is system key parameter
|
static SpreadsheetData.ParameterStatus |
USER_KEY
Key parameter analyzed from spreadsheet search
|
Modifier and Type | Method and Description |
---|---|
static SpreadsheetData.ParameterStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpreadsheetData.ParameterStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpreadsheetData.ParameterStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final SpreadsheetData.ParameterStatus LOCK
public static final SpreadsheetData.ParameterStatus SYSTEM_KEY
public static final SpreadsheetData.ParameterStatus USER_KEY
public static final SpreadsheetData.ParameterStatus HIDE_STATUS
public static final SpreadsheetData.ParameterStatus SCALE_ITEM
public static final SpreadsheetData.ParameterStatus READ_ONLY
public static final SpreadsheetData.ParameterStatus MODIFIED
public static final SpreadsheetData.ParameterStatus FORCE_COLOR
public static final SpreadsheetData.ParameterStatus HIDDEN_VALUE
public static final SpreadsheetData.ParameterStatus OPTION_VALUE
public static final int _LOCK
public static final int _SYSTEM_KEY
public static final int _USER_KEY
public static final int _HIDE_STATUS
public static final int _SCALE_ITEM
public static final int _READ_ONLY
public static final int _MODIFIED
public static final int _FORCE_COLOR
public static final int _HIDDEN_VALUE
public static final int _OPTION_VALUE
public static SpreadsheetData.ParameterStatus valueOf(int value)
public static SpreadsheetData.ParameterStatus valueOf(String name)
public static SpreadsheetData.ParameterStatus[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.