public static class SpecialPiercingInsertBuilder.PunchOrDieTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIE |
static int |
_DIE_CAVITY_AND_SLUG_HOLE |
static int |
_PUNCH |
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
DIE |
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
DIE_CAVITY_AND_SLUG_HOLE |
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
PUNCH |
Modifier and Type | Method and Description |
---|---|
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpecialPiercingInsertBuilder.PunchOrDieTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final SpecialPiercingInsertBuilder.PunchOrDieTypes PUNCH
public static final SpecialPiercingInsertBuilder.PunchOrDieTypes DIE
public static final SpecialPiercingInsertBuilder.PunchOrDieTypes DIE_CAVITY_AND_SLUG_HOLE
public static final int _PUNCH
public static final int _DIE
public static final int _DIE_CAVITY_AND_SLUG_HOLE
public static SpecialPiercingInsertBuilder.PunchOrDieTypes valueOf(int value)
public static SpecialPiercingInsertBuilder.PunchOrDieTypes valueOf(String name)
public static SpecialPiercingInsertBuilder.PunchOrDieTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.