public static class SolidPatchBuilder.SolidPatchType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LINK_BODY
Link body type indicates to create link body
|
static int |
_SOLID_PATCH
Solid patch type indicates to create solid patch
|
static SolidPatchBuilder.SolidPatchType |
LINK_BODY
Link body type indicates to create link body
|
static SolidPatchBuilder.SolidPatchType |
SOLID_PATCH
Solid patch type indicates to create solid patch
|
Modifier and Type | Method and Description |
---|---|
static SolidPatchBuilder.SolidPatchType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SolidPatchBuilder.SolidPatchType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SolidPatchBuilder.SolidPatchType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SolidPatchBuilder.SolidPatchType SOLID_PATCH
public static final SolidPatchBuilder.SolidPatchType LINK_BODY
public static final int _SOLID_PATCH
public static final int _LINK_BODY
public static SolidPatchBuilder.SolidPatchType valueOf(int value)
public static SolidPatchBuilder.SolidPatchType valueOf(String name)
public static SolidPatchBuilder.SolidPatchType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.