public interface RemoveHolesBuilder extends Builder
ProgressiveDieManager.createRemoveHolesBuilder()
Property | Value |
---|---|
MergeOutput | 0 |
SelectionType | Body |
Modifier and Type | Interface and Description |
---|---|
static class |
RemoveHolesBuilder.SelectionTypes
select object types, body or face
|
Modifier and Type | Method and Description |
---|---|
void |
addHolesData(Edge[] edges,
Face[] faces)
Add the hole data
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
ScCollector |
bodySelection()
Returns the body selection
License requirements: None. |
void |
clearHoleData()
Clear all the hole data that was input to the builder.
|
ScCollector |
faceToPatch()
Returns the face to patch
License requirements: None. |
ScCollector |
holeFace()
Returns the hole faces
License requirements: None. |
boolean |
mergeOutput()
Returns the reduce number of output features setting
License requirements: None. |
void |
removeHoleData(String holeName)
Remove the hole from hole data from builder.
|
RemoveHolesBuilder.SelectionTypes |
selectionType()
Returns the selection type
License requirements: None. |
void |
setHighlight(NXObject object,
boolean highlight)
Set object highlight or unhighlight.
|
void |
setMergeOutput(boolean mergeOutput)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
void |
setSelectionType(RemoveHolesBuilder.SelectionTypes selType)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
RemoveHolesBuilder.SelectionTypes selectionType() throws NXException, RemoteException
NXException
RemoteException
void setSelectionType(RemoveHolesBuilder.SelectionTypes selType) throws NXException, RemoteException
selType
- NXException
RemoteException
ScCollector bodySelection() throws NXException, RemoteException
NXException
RemoteException
ScCollector faceToPatch() throws NXException, RemoteException
NXException
RemoteException
ScCollector holeFace() throws NXException, RemoteException
NXException
RemoteException
void addHolesData(Edge[] edges, Face[] faces) throws NXException, RemoteException
edges
- the edges of the holes informationfaces
- the faces of the holes informationNXException
RemoteException
void setHighlight(NXObject object, boolean highlight) throws NXException, RemoteException
object
- the object to highlight or unhighlight.highlight
- the status to highlight or unhighlight.NXException
RemoteException
void removeHoleData(String holeName) throws NXException, RemoteException
holeName
- the hole nameNXException
RemoteException
void clearHoleData() throws NXException, RemoteException
NXException
RemoteException
boolean mergeOutput() throws NXException, RemoteException
NXException
RemoteException
void setMergeOutput(boolean mergeOutput) throws NXException, RemoteException
mergeOutput
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.