public static class PunchInsertBuilder.PunchPocketTypeItemsStripperPlate extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CIRCLE
Punch pocket type in stripper plate is circle
|
static int |
_CLEARANCE
Punch pocket type in stripper plate is clearance
|
static int |
_FILLET
Punch pocket type in stripper plate is fillet
|
static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate |
CIRCLE
Punch pocket type in stripper plate is circle
|
static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate |
CLEARANCE
Punch pocket type in stripper plate is clearance
|
static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate |
FILLET
Punch pocket type in stripper plate is fillet
|
Modifier and Type | Method and Description |
---|---|
static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate[] |
values()
Returns an array that contains the values for this enum.
|
public static final PunchInsertBuilder.PunchPocketTypeItemsStripperPlate CLEARANCE
public static final PunchInsertBuilder.PunchPocketTypeItemsStripperPlate FILLET
public static final PunchInsertBuilder.PunchPocketTypeItemsStripperPlate CIRCLE
public static final int _CLEARANCE
public static final int _FILLET
public static final int _CIRCLE
public static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate valueOf(int value)
public static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate valueOf(String name)
public static PunchInsertBuilder.PunchPocketTypeItemsStripperPlate[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.