public static class PiercingInsertBuilder.DieInsertTypeItems extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BACKING_INSERT
the backing insert type
|
static int |
_DIE_INSERT
the die insert type
|
static PiercingInsertBuilder.DieInsertTypeItems |
BACKING_INSERT
the backing insert type
|
static PiercingInsertBuilder.DieInsertTypeItems |
DIE_INSERT
the die insert type
|
Modifier and Type | Method and Description |
---|---|
static PiercingInsertBuilder.DieInsertTypeItems |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PiercingInsertBuilder.DieInsertTypeItems |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PiercingInsertBuilder.DieInsertTypeItems[] |
values()
Returns an array that contains the values for this enum.
|
public static final PiercingInsertBuilder.DieInsertTypeItems DIE_INSERT
public static final PiercingInsertBuilder.DieInsertTypeItems BACKING_INSERT
public static final int _DIE_INSERT
public static final int _BACKING_INSERT
public static PiercingInsertBuilder.DieInsertTypeItems valueOf(int value)
public static PiercingInsertBuilder.DieInsertTypeItems valueOf(String name)
public static PiercingInsertBuilder.DieInsertTypeItems[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.