public static class LsdynaGeometryPreparationBuilder.DrawType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DOUBLE_DRAW
For draw die, punch and binder are higher than die.
|
static int |
_SINGLE_DRAW
For draw die, punch and binder are lower than die.
|
static LsdynaGeometryPreparationBuilder.DrawType |
DOUBLE_DRAW
For draw die, punch and binder are higher than die.
|
static LsdynaGeometryPreparationBuilder.DrawType |
SINGLE_DRAW
For draw die, punch and binder are lower than die.
|
Modifier and Type | Method and Description |
---|---|
static LsdynaGeometryPreparationBuilder.DrawType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.DrawType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.DrawType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LsdynaGeometryPreparationBuilder.DrawType SINGLE_DRAW
public static final LsdynaGeometryPreparationBuilder.DrawType DOUBLE_DRAW
public static final int _SINGLE_DRAW
public static final int _DOUBLE_DRAW
public static LsdynaGeometryPreparationBuilder.DrawType valueOf(int value)
public static LsdynaGeometryPreparationBuilder.DrawType valueOf(String name)
public static LsdynaGeometryPreparationBuilder.DrawType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.