public static class InitProjectBuilder.MaterialId extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
None material is set
|
static int |
_NYLON
Nylon material type
|
static InitProjectBuilder.MaterialId |
NONE
None material is set
|
static InitProjectBuilder.MaterialId |
NYLON
Nylon material type
|
Modifier and Type | Method and Description |
---|---|
static InitProjectBuilder.MaterialId |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InitProjectBuilder.MaterialId |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InitProjectBuilder.MaterialId[] |
values()
Returns an array that contains the values for this enum.
|
public static final InitProjectBuilder.MaterialId NONE
public static final InitProjectBuilder.MaterialId NYLON
public static final int _NONE
public static final int _NYLON
public static InitProjectBuilder.MaterialId valueOf(int value)
public static InitProjectBuilder.MaterialId valueOf(String name)
public static InitProjectBuilder.MaterialId[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.