public interface FaceSplitBuilder extends Builder
FaceSplitCollection.createFaceSplitBuilder()
Property | Value |
---|---|
Tolerance | 0.025 |
Modifier and Type | Interface and Description |
---|---|
static class |
FaceSplitBuilder.FaceSplitType
the type for Split Face
|
Modifier and Type | Method and Description |
---|---|
Curve[] |
createIsoclines(Face[] pFacesToDivide)
Create isocline
License requirements: None. |
ScCollector |
divObjects()
Returns the dividing objects which will be different according to the split type
License requirements: None. |
ScCollector |
faceToDivide()
Returns the faces to be divided
License requirements: None. |
void |
findMoldUnsplitFace()
Set the reference point to the selected face center.
|
void |
setTolerance(double tolerance)
License requirements: None. |
void |
setType(FaceSplitBuilder.FaceSplitType splitType)
License requirements: None. |
double |
tolerance()
Returns the tolerance is used to do dividing face operation
License requirements: None. |
FaceSplitBuilder.FaceSplitType |
type()
Returns the split face type which splits a face by using curves, edges, plane, face, isolines or
intersected curves with another body
License requirements: None. |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
FaceSplitBuilder.FaceSplitType type() throws NXException, RemoteException
NXException
RemoteException
void setType(FaceSplitBuilder.FaceSplitType splitType) throws NXException, RemoteException
splitType
- NXException
RemoteException
ScCollector faceToDivide() throws NXException, RemoteException
NXException
RemoteException
ScCollector divObjects() throws NXException, RemoteException
NXException
RemoteException
double tolerance() throws NXException, RemoteException
NXException
RemoteException
void setTolerance(double tolerance) throws NXException, RemoteException
tolerance
- NXException
RemoteException
Curve[] createIsoclines(Face[] pFacesToDivide) throws NXException, RemoteException
pFacesToDivide
- faces to be divided with isoclinesNXException
RemoteException
void findMoldUnsplitFace() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.