public static class ElectrodeBlankBuilder.BlankMaterial extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COPPER
the material of the blank is copper
|
static int |
_GRAPHITE
the material of the blank is graphite
|
static ElectrodeBlankBuilder.BlankMaterial |
COPPER
the material of the blank is copper
|
static ElectrodeBlankBuilder.BlankMaterial |
GRAPHITE
the material of the blank is graphite
|
Modifier and Type | Method and Description |
---|---|
static ElectrodeBlankBuilder.BlankMaterial |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElectrodeBlankBuilder.BlankMaterial |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElectrodeBlankBuilder.BlankMaterial[] |
values()
Returns an array that contains the values for this enum.
|
public static final ElectrodeBlankBuilder.BlankMaterial COPPER
public static final ElectrodeBlankBuilder.BlankMaterial GRAPHITE
public static final int _COPPER
public static final int _GRAPHITE
public static ElectrodeBlankBuilder.BlankMaterial valueOf(int value)
public static ElectrodeBlankBuilder.BlankMaterial valueOf(String name)
public static ElectrodeBlankBuilder.BlankMaterial[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.