public static class DieCavityAndSlugHoleBuilder.ClearanceOptionItems extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONSTANT
The design option is normal
|
static int |
_VARIABLE
The design option is fineblanking
|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
CONSTANT
The design option is normal
|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
VARIABLE
The design option is fineblanking
|
Modifier and Type | Method and Description |
---|---|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems[] |
values()
Returns an array that contains the values for this enum.
|
public static final DieCavityAndSlugHoleBuilder.ClearanceOptionItems CONSTANT
public static final DieCavityAndSlugHoleBuilder.ClearanceOptionItems VARIABLE
public static final int _CONSTANT
public static final int _VARIABLE
public static DieCavityAndSlugHoleBuilder.ClearanceOptionItems valueOf(int value)
public static DieCavityAndSlugHoleBuilder.ClearanceOptionItems valueOf(String name)
public static DieCavityAndSlugHoleBuilder.ClearanceOptionItems[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.