public static class BlankNestingBuilder.LayoutTypeSpecification extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE_UP
Auto-position blank along x-axis without bounding box.
|
static int |
_PARALLELOGRAM
Auto-position blank along x-axis with parallelogram bounding box.
|
static int |
_RECTANGLE
Auto-position blank along x-axis with rectangle bounding box.
|
static int |
_TRAPEZOID
Rotate blank 180 degrees and auto-position it along x-axis with trapezoid bounding box.
|
static int |
_TWO_PAIR
Two pair without bounding box.
|
static int |
_TWO_UP
Two up without bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
ONE_UP
Auto-position blank along x-axis without bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
PARALLELOGRAM
Auto-position blank along x-axis with parallelogram bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
RECTANGLE
Auto-position blank along x-axis with rectangle bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
TRAPEZOID
Rotate blank 180 degrees and auto-position it along x-axis with trapezoid bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
TWO_PAIR
Two pair without bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
TWO_UP
Two up without bounding box.
|
Modifier and Type | Method and Description |
---|---|
static BlankNestingBuilder.LayoutTypeSpecification |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlankNestingBuilder.LayoutTypeSpecification |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlankNestingBuilder.LayoutTypeSpecification[] |
values()
Returns an array that contains the values for this enum.
|
public static final BlankNestingBuilder.LayoutTypeSpecification RECTANGLE
public static final BlankNestingBuilder.LayoutTypeSpecification PARALLELOGRAM
public static final BlankNestingBuilder.LayoutTypeSpecification TRAPEZOID
public static final BlankNestingBuilder.LayoutTypeSpecification ONE_UP
public static final BlankNestingBuilder.LayoutTypeSpecification TWO_UP
public static final BlankNestingBuilder.LayoutTypeSpecification TWO_PAIR
public static final int _RECTANGLE
public static final int _PARALLELOGRAM
public static final int _TRAPEZOID
public static final int _ONE_UP
public static final int _TWO_UP
public static final int _TWO_PAIR
public static BlankNestingBuilder.LayoutTypeSpecification valueOf(int value)
public static BlankNestingBuilder.LayoutTypeSpecification valueOf(String name)
public static BlankNestingBuilder.LayoutTypeSpecification[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.