Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.sim |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation.
|
Class and Description |
---|
KinematicConfigurator
Represents the ISV base class object
To obtain an instance of this class, use Part.kinematicConfigurator() Created in NX7.5.0 |
Class and Description |
---|
ArchiveImportBuilder
Represents a ArchiveImportBuilder builder object.
|
Breakpoint
Represents the Breakpoint class object
Use the NcProgramManagerBuilder class to create a Breakpoint object. |
ExportMachineKitBuilder
This class is used for the Export Machine Kit Dialog.
|
ImportMachineKitBuilder
This class is used for the Import Machine Kit Dialog.
|
IsvControlPanelBuilder
Represents a
IsvControlPanelBuilder
To create a new instance of this class, use KinematicConfigurator.createIsvControlPanelBuilder(nxopen.sim.IsvControlPanelBuilder.VisualizationType, nxopen.cam.CAMObject[]) Created in NX8.0.0 |
IsvControlPanelBuilder.DetailType
Type of record reported in the Simulation Details group
|
IsvControlPanelBuilder.IsInHistoryBufferCb
Prototype for IsInHistoryBufferChanged callbacks
|
IsvControlPanelBuilder.MachineControlReadVariableData
This class holds the data returned from
IsvControlPanelBuilder.machineControlReadVariable(java.lang.String, java.lang.String) |
IsvControlPanelBuilder.PostprocessorFilenameData
This class holds the data returned from
IsvControlPanelBuilder.getPostprocessorFilename() |
IsvControlPanelBuilder.SimStopCb
Prototype for SimStop callbacks
|
IsvControlPanelBuilder.SingleStepModeType
The Single Step Mode type that used in
IsvControlPanelBuilder.VisualizationType.MACHINE_CODE_SIMULATE_CSE simulation mode. |
IsvControlPanelBuilder.SingleStepType
The Single Step type that used in
IsvControlPanelBuilder.VisualizationType.MACHINE_CODE_SIMULATE_MTD or
IsvControlPanelBuilder.VisualizationType.TOOL_PATH_SIMULATION simulation mode. |
IsvControlPanelBuilder.VisualizationType
The Visualization type
|
IsvControlPanelBuilder.VncMode
Type of VNC Mode
|
IsvControlPanelBuilder.VncStatusCb
Prototype for VNC Status callbacks
|
KinematicAxis
Represents the SimKimAxis class object
Use the KinematicAxisBuilder class to create a KinematicAxis object. |
KinematicAxisBuilder
Represents the SimKimAxisBuilder class object
Use the KinematicConfigurator class to create a KinematicAxisBuilder object. |
KinematicAxisBuilder.AxisDirectionType
The axis direction type
|
KinematicAxisBuilder.AxisMotionType
The axis motions type
|
KinematicChain
This class is used for add kinematic chain to the list.
|
KinematicChain.CoordinatePlaneTypes
Represents the coordinate plane type
|
KinematicChain.Types
Represents the kinematic chain type
|
KinematicChainConfiguration
This class is used for define kinematic chains.
|
KinematicChainList
Represents a list of objects.
|
KinematicChannelBuilder
This class is used for add kinematic channel to the channel configuratation list.
|
KinematicChannelBuilderList
Represents a list of objects.
|
KinematicChannelConfigurationBuilder
This class is used for channel configuration.
|
KinematicComponent
Represents the KinematicComponent class object
Use the KinematicConfigurator class to create a KinematicComponent object. |
KinematicComponentBuilder
Represents the KinamaticComponentBuilder class object
To create a new instance of this class, use KinematicComponentCollection.createHeadBaseComponentBuilder(nxopen.sim.KinematicComponent) Created in NX7.5.0 |
KinematicComponentBuilder.RegisterTypes
The register types
|
KinematicComponentBuilder.SystemClass
The SIM KIM system classes
|
KinematicComponentBuilder.WorkPositionAngleTypes
The Working Position Angle type
|
KinematicComponentCollection
Represents the SimKimComponent Collection
To obtain an instance of this class, refer to KinematicConfigurator Created in NX7.5.0 |
KinematicConfigurator.FindAxisData
This class holds the data returned from
KinematicConfigurator.findAxis(java.lang.String) |
KinematicConfigurator.UniteTypes
The unite types for spinning geometries
|
KinematicImportMcfBuilder
Represents a builder for an import axis and channel data from mcf
Use the Part class to create a KinematicImportMcfBuilder object. |
KinematicJunction
Represents the KinematicJunction class object
Use the KinematicConfigurator class to create a SimKimJunction object. |
KinematicJunctionBuilder
Represents the SimKimJunctionBuilder class object
Use the KinematicConfigurator class to create a KinematicJunctionBuilder object. |
KinematicJunctionBuilder.SystemClass
The junction system classes
|
KinematicJunctionBuilderList
Represents a list of objects.
|
KinematicModel
Represents the Kinematic Model class object.
|
KinematicSinumerikCaBuilder
This class is used for edit sinumerik collision avoidance properties.
|
KinematicSinumerikCaBuilder.PlcInitStateTypes
The init state types
|
KinematicSinumerikCaBuilder.PlcUsageTypes
The usage types
|
MachineKitBuilder
This class is used for the Machine Kit Create Dialog.
|
MachineLibraryBuilder
This class is used for the Machine Library Dialog.
|
MachineToolConfiguration
Represents a Machine Tool Configuration object.
|
MachineToolConfiguration.ControllerLines
The controller line
|
MachineToolConfiguration.MdynamicsTypes
The mdynamics types
|
MachineToolConfiguration.PlaneTypes
The plane selection types
|
MachineToolConfiguration.SwivelingTypes
The machine swiveling types
|
MachineToolConfiguration.TechnologyTypes
The machine technology types
|
MachineToolConfiguration.UnitTypes
The units type
|
NcChannelSelectionData
Represents the NcChannelSelectionData class object
Use the NcChannelSelectionData class to create a NcChannelSelectionData object. |
NcProgram
Represents the NcProgram class object
Use the NcProgramManagerBuilder class to create a NcProgram object. |
NcProgramManagerBuilder
Represents a NcProgramManagerBuilder builder object.
|
SimDebugBuilder
Represents a
SimDebugBuilder
To create a new instance of this class, use KinematicConfigurator.createSimDebugBuilder() Created in NX8.0.0 |
SimDebugBuilder.DriverType
Represents the driver type
|
SimDebugBuilder.DumpType
Represents the dump type
|
SimDebugBuilder.KinematicModelType
Represents the kinematic model type
|
SimDebugBuilder.OutputType
The output type
|
SimDebugBuilder.PrintoutTagsOrPointersType
Represents the printout tags or pointers type
|
SimDebugBuilder.TraceType
Represents the trace type
|
SimDebugBuilder.UiType
Represents the ui type
|
SinumerikCaExportBuilder
This class is used for export a spf file.
|
SinumerikCaFacetBuilder
This class is used for set the facet tolerance.
|
SinumerikCaPlaceholderBuilder
This class is used for select or unselect component of the placeholder tools.
|
SinumerikCaSimplifyBodiesBuilder
This class is used for replace geometry.
|
SinumerikCaSimplifyBodiesBuilder.CloseGapTypes
Represents the close gap types
|
SinumerikCaSimplifyBodiesBuilder.ObjectToReplaceWithTypes
The object to replaces with types
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.