public static class MachineToolConfiguration.UnitTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_IN
The inch unit type
|
static int |
_MM
The millimeter unit type
|
static MachineToolConfiguration.UnitTypes |
IN
The inch unit type
|
static MachineToolConfiguration.UnitTypes |
MM
The millimeter unit type
|
Modifier and Type | Method and Description |
---|---|
static MachineToolConfiguration.UnitTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MachineToolConfiguration.UnitTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MachineToolConfiguration.UnitTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final MachineToolConfiguration.UnitTypes MM
public static final MachineToolConfiguration.UnitTypes IN
public static final int _MM
public static final int _IN
public static MachineToolConfiguration.UnitTypes valueOf(int value)
public static MachineToolConfiguration.UnitTypes valueOf(String name)
public static MachineToolConfiguration.UnitTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.