public static class KinematicComponentBuilder.RegisterTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SAME_AS_POCKET_ID
the pocket id defined the register
|
static int |
_SPECIFY
the register is specified
|
static KinematicComponentBuilder.RegisterTypes |
SAME_AS_POCKET_ID
the pocket id defined the register
|
static KinematicComponentBuilder.RegisterTypes |
SPECIFY
the register is specified
|
Modifier and Type | Method and Description |
---|---|
static KinematicComponentBuilder.RegisterTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static KinematicComponentBuilder.RegisterTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static KinematicComponentBuilder.RegisterTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final KinematicComponentBuilder.RegisterTypes SAME_AS_POCKET_ID
public static final KinematicComponentBuilder.RegisterTypes SPECIFY
public static final int _SAME_AS_POCKET_ID
public static final int _SPECIFY
public static KinematicComponentBuilder.RegisterTypes valueOf(int value)
public static KinematicComponentBuilder.RegisterTypes valueOf(String name)
public static KinematicComponentBuilder.RegisterTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.